Skip to main content

Product Longevity Program (PLP)

The Renesas Product Longevity Program (PLP) helps customers select the most appropriate part for applications that require long life cycles.

In limited cases, a PLP product may be replaced by an equivalent product. These products will be listed here for about three months following the date of the change.

Program Overview

  1. Products participating in the PLP are selected from products developed for industrial and infrastructure market segments. Products participating in the PLP are expected to have a long product life.
  2. A PLP product is managed under a special product life cycle for the duration that it participates in the program. Renesas Electronics strives to maintain supply of a PLP product for the duration that it participates in the program. Following the termination of a product's participation in the PLP, life cycle management for the product will be carried out as a regular product.

    An Example of a PLP Product's Supply Period (with PLP termination date of December 2024)

  3. PLP products are indicated clearly on the website, and the PLP duration is also published.
  4. The PLP duration is current at the time of publishing. It may be extended due to circumstances.
  5. Due to various circumstances, in some cases a PLP product may be replaced by an equivalent product that is also in the PLP. Products to which this applies will be indicated in a list published here for about three months following the change.
  6. By using this program, you understand and agree to the terms for using this website (Using Our Website) and the important notes about the PLP.

Applicable Products

Products from Renesas' main product categories (microcontrollers and microprocessors, analog devices, power devices, compound semiconductor devices, memory, ASSP, etc.) that meet the following conditions are managed under a special product life cycle as PLP products.

  1. The product is developed for the industrial or infrastructure markets (including some general markets)
  2. The product is published on the Renesas website (products developed for a special segment or a specific customer, etc. are excluded)
  3. Future supply of the product for a fixed period is possible in terms of production facilities and other factors
  4. The product's status is "mass production" at the time it joins the program
    Note 1. Whether a product participates in the PLP is determined after its status changes from under development to mass production.
    Note 2. The PLP includes products that are "not recommended for new design" but are being supplied specially to customers who have already adopted them. Please refer to the Supply Policy page.
ProductMain applicable products
MicrocontrollersRA, RZ, RX, RL78, SH, V850, R8C, 78K, H8SX, H8S, H8, M16C, M32C, etc.
Other MCUs & MPUs

SuperH RISC engine Family
SH7124, SH7125, SH7046, SH7148, SH7101, SH7048, SH7104, SH7106, SH7108, SH7047, SH7049, SH7105, SH7107, SH7109, SH7083, SH7084, SH7085, SH7086, SH7131, SH7132, SH7136, SH7137, SH7144, SH7145, SH7146, SH7149, SH7203, SH7206, SH7211, SH7214, SH7216, SH7239, SH7237, SH7243, SH7262, SH7264, SH7263, SH7266, SH7267, SH7268, SH7269, SH726A, SH726B, SH7285, SH7286, SH7705, SH7706, SH7709S, SH7720, SH7721, SH7727, SH7750R, SH7751R, SH7760, SH7722, SH7723, SH7730, SH7731, SH7734, SH7764, SH7780, SH7670

V850 Family
V850E/IA3, V850E/IA4, V850E/IF3, V850E/IG3, V850E/IG4, V850E/IH4, V850E/IG4-H, V850E/IH4-H, V850E/MA3, V850E2/Mx4, V850ES/Hx3, V850ES/IE2, V850ES/IK1, V850ES/Jx3, V850ES/Jx3-E, V850ES/Jx3-H, V850ES/Jx3-L, V850ES/Jx3-L, V850ES/Jx3-U

R8C Family
R8C/18, R8C/19, R8C/1A, R8C/1B, R8C/24, R8C/25, R8C/26, R8C/27, R8C/33C, R8C/33D, R8C/33M, R8C/33T, R8C/34C, R8C/34M, R8C/35C, R8C/35D, R8C/35M, R8C/36C, R8C/36M, R8C/36T-A, R8C/38C, R8C/38M, R8C/3GC, R8C/L35C, R8C/L35M, R8C/L36C, R8C/L36M, R8C/L38C, R8C/L38M, R8C/L3AC, R8C/L3AM

M16C Family (R32C / M32C / M16C)
M16C/62P, M16C/63, M16C/64A, M16C/64C, M16C/65, M16C/65C, M16C/6C, R32C/116, R32C/117, R32C/118, R32C/116A, R32C/117A, R32C/118A

H8 Family
H8/3029, H8/3048B, H8/3052B, H8/3060, H8/3061, H8/3062, H8/3068, H8/38076R, H8/38537, H8/38776, H8/36014, H8/36024, H8/36049, H8/3672, H8/3687, H8/3802, H8/38002S, H8/38004, H8/38104, H8/3827R, H8/3827S, H8/38327, H8/38427

H8S Family
H8S/2125, H8S/2138, H8S/2134, H8S/2144B, H8S/2134B, H8S/2148, H8S/2144, H8S/2164, H8S/2168, H8S/2215, H8S/2218, H8S/2212, H8S/2258, H8S/2239, H8S/2238, H8S/2237, H8S/2227, H8S/2268, H8S/2264, H8S/2319, H8S/2329, H8S/2339, H8S/2368, H8S/2378, H8S/2378R, H8S/2398, H8S/2357, H8S/2426, H8S/2426R, H8S/2424, H8S/2427, H8S/2427R, H8S/2425, H8S/2456, H8S/2456R, H8S/2454, H8S/2472, H8S/2463, H8S/2462, H8S/2556, H8S/2552, H8S/2506, H8S/2668, H8S/20203R, H8S/20215R, H8S/20223R, H8S/20235R, H8S/20323R, H8S/20335R

H8SX Family
H8SX/1635, H8SX/1635L, H8SX/1638, H8SX/1638L, H8SX/1645, H8SX/1645L, H8SX/1648A, H8SX/1648L, H8SX/1650, H8SX/1651, H8SX/1653, H8SX/1655, H8SX/1655M, H8SX/1657, H8SX/1658R, H8SX/1658M, H8SX/1663, H8SX/1665, H8SX/1665M, H8SX/1668R, H8SX/1668M

78K Family
78K0/Ix2, 78K0/Kx2, 78K0/Kx2-A, 78K0/Kx2-C, 78K0/Kx2-L, 78K0/Lx3, 78K0R/Ix3, 78K0R/Kx3, 78K0R/Kx3-A, 78K0R/Kx3-C, 78K0R/Kx3-L, 78K0R/Kx3-L, 78K0R/Lx3

Renesas Synergy™ PlatformRenesas Synergy Microcontrollers S7 Series, Renesas Synergy Microcontrollers S5 Series, Renesas Synergy Microcontrollers S3 Series, Renesas Synergy Microcontrollers S1 Series
Analog devices (mixed signal)SRAM, EEPROM, op-amp, etc.
Power devicesIGBTs, MOSFETs, DC/DC Converters, Linear Regulators (LDO), DC/DC Power Modules, FET & Motor Drivers, Digital Power, Smart Power Stages, etc.
Compound semiconductor devicesOptoelectronics
ASSPR-IN32M3, etc.
Former-Dialog ProductsDA*, SLG*, SC14*, AT*
Current Sense AmplifiersISL28006, ISL28022
Operational AmplifiersISL28130, ISL28133, ISL28134, ISL28230, ISL28233, ISL28291, ISL28430, ISL28433
TransceiversISL3152E, ISL3156E, ISL3158E, ISL3159E, ISL3170E, ISL3172E, ISL3176E, ISL3178E, ISL3179E, ISL32452E, ISL32485E, ISL32495E, ISL41334, ISL81387, ISL81487, ISL83072E, ISL83080E, ISL83083E, ISL83483, ISL83485, ISL84051, ISL8485, ISL8487E
Voltage ReferencesISL21010, ISL21080, ISL60002
MRAMM30042040108X0IM30042040108X0PM30082040108X0PM30162040108X0PM10162040108X0P
M3016316035NX0IM3032316035NX0I
NFCPTX100R, PTX105R, PTX130R
Clocks & Timing

VersaClock Family
5L35021, 5L35023, 5P35021, 5P35023, 5P49V60, 5P49V6965, 5P49V6967, 5P49V6968, 5P49V6975, 9FGV1001, 9FGV1002, 9FGV1004, 9FGV1005, 9FGV1006, 9FGV1008, RC210, RC310

FemtoClock Family
RC223, RC22504A, RC22514A, RC32012A, RC32112A, RC323, RC32504A, RC32514A

Clock Buffer Family
9DBL0242, 9DBL0252, 9DBL0442, 9DBL0452, 9DBL0641, 9DBL0651, 9DBL0841, 9DBL0851, 9DBV0231, 9DBV0241, 9DBV0431, 9DBV0441, 9DBV0531, 9DBV0541, 9DBV0641, 9DBV0831, 9DBV0841, RC19002, RC19004, RC19008, RC19013, RC19016, RC19020, RC19024, RC19104A, RC19108A, RC19202, RC19204, RC19208, RC19216

Oscillator Family
XF, XK, XP, XT

Lists

List of Changed PLP Products

Changed PLP products will be listed here for about three months following the date of the change.

List of Changed PLP Products (PDF)

List of Products Terminated from PLP

Due to changes made in our material supplier's production policy or other reasons, participation of some of the products in the program is terminated in consideration of the effect it may cause on QCD (Quality, Cost and Delivery). Renesas Electronics understands that the PLP plays an important role for our customers in selecting a part.

Renesas Electronics will make the utmost effort to provide all related information immediately after any changes occur that may affect PLP participating products.

List of Products Terminated from PLP (XLSX)

Important Notes

Before using this program, please read and understand the following.

  1. All the information about this program is published only on the website. A record of changes is also published. Please check it regularly.
  2. This program provides an indication of the supply period of a product.
  3. The participation of a product in the program, its date of termination, and the contents of the program itself may be subject to change due to circumstances beyond our control. If any change occurs, it will be published on the website.
  4. PCN (Product Change Notices) for changes in product specifications, manufacturing facilities, or materials may be issued due to circumstances beyond our control even while this program is in effect.
  5. Even while this program is in effect, a PLP product may be replaced by another (equivalent) product in the program. Products to which this applies will be indicated in a list published on the website for about three months following the change.
  6. For some products such as memory, customers will be expected to switch to a compatible product even while this program is in effect.
  7. The date of PLP termination is the date that was planned at the point in time when it was officially announced. It is subject to change.