Skip to main content

IDT Expands VersaClock 5 Family to include Devices with Additional Outputs Supporting PCI Express Timing

The Latest Versions of the Leading Programmable Clock Generator Reduce Board Space and BOM for Designs Requiring Multiple PCIe Clocks

July 16, 2015

SAN JOSE, Calif., June 30, 2015 – Integrated Device Technology, Inc. (IDT®) (NASDAQ: IDTI) announced today the expansion of its VersaClock® 5 family of programmable clock generators with new devices that simplify the creation of PCI Express® clocks while providing the flexible outputs for which VersaClock is known. The new members of the high-performance VersaClock 5 family feature dedicated low-power HCSL (LP-HCSL) outputs that reduce board space and bill of materials (BOM) by providing an integrated clock generation and distribution solution for PCIe designs.

The 5P49V5907 and 5P49V5908 devices have three outputs that can generate any frequency up to 350 MHz in various output types, and an additional four or eight LP-HCSL outputs specifically for PCIe clocking. They possess the same best-in-class jitter and power performance as the original 5P49V5901 device.

“IDT continues to develop technology that enables engineers to build highly flexible low-power timing systems with ultra-compact footprints,” said Kris Rausch, general manager of IDT’s multi-market timing division. “With these new devices, design teams building PCIe-based systems enjoy the superior performance of the original VersaClock 5 device as well as tighter integration that shrinks board space and BOM.”

VersaClock 5 programmable timing devices feature excellent jitter performance at half the power of competing devices. With RMS phase jitter of less than 0.7 picoseconds over the full 12 kHz to 20 MHz integration range, the products are ideal for such markets as high-end consumer, networking, computing, industrial and communications.

Pricing and Availability

The 5P49V5907 and 5P49V5908 products are available now in 1,000-part lots at a per-unit price of $5.5 and $6.5 respectively.

About IDT Clock and Timing Solutions

With a product portfolio 10 times greater and broader than any other, IDT is the world’s leader in silicon timing and is in a unique position to address the needs of virtually any application. With the industry’s largest market share, IDT is the only one-stop-shop for timing, offering products from full-featured system solutions to simple clock building-block devices. Factory-programmable options and clock solution customization capabilities address unique customer requirements, while the lowest jitter and lowest power features set IDT apart from the competition. Products are accompanied by a world-class support team driven by service and responsiveness goals. For more information about IDT’s leading portfolio of timing products, please visit http://www.idt.com/go/timing.

About IDT

Integrated Device Technology, Inc. develops system-level solutions that optimize its customers’ applications. IDT uses its market leadership in timing, serial switching and interfaces, and adds analog and system expertise to provide complete application-optimized, mixed-signal solutions for the communications, computing and consumer segments. Headquartered in San Jose, Calif., IDT has design, manufacturing, sales facilities and distribution partners throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com. Follow IDT on Facebook, LinkedIn, Twitter, YouTube and Google+.

Share this news on