Skip to main content

IDT Memory Interface Devices Qualified for DDR4 Enterprise DIMMs on Intel Xeon Processor E5-2600 v4 Product Family-Based Systems

The Latest IDT Chipset Extends the Company’s Leadership in DDR4 Performance, Latency and Power Optimization

April 5, 2016

SAN JOSE, Calif., April 5, 2016 — Integrated Device Technology, Inc. (IDT®) (NASDAQ: IDTI) today announced that its 4RCD0124K register, 4DB0226KA3 data buffer and TSE2004 temperature sensor components are fully qualified by memory eco-system leaders,  including Intel, Dell and Micron, for DIMM applications on Intel® Xeon® processor E5-2600 v4 product family-based server and storage systems.

“Mission #1 for IDT is to push the memory performance and capacity envelope by addressing profound challenges in signal integrity, capacity scaling and fault isolation and correction,” said Rami Sethi, vice president and general manager of IDT’s memory interface products. “We have worked closely with industry leaders such as Dell, Intel and Micron to validate and qualify our components for DIMM applications on Intel Xeon processor E5-2600 v4 product family-based OEM systems. The result is huge performance gains that benefit a wide range of end user applications such as real-time data analytics, online transaction processing and workload virtualization.”

“Intel and IDT have a wide-ranging engagement on strategic and near-term activities including JEDEC specifications and product qualification,” said Jennifer Huffstetler, director of product marketing in Intel’s Data Center Group. “Intel has worked closely with IDT to validate and qualify their register, data buffer and temperature sensor components with the Intel Xeon processor E5 v4 product family to deliver excellent memory performance to our OEM customers.”

IDT's register component enables registered DIMM (RDIMM)-based systems to deliver industry-leading performance per watt.  In conjunction with the register, IDT’s data buffers allow up to 3 TB of memory capacity when fully populated with 128GB/64GB/32GB LRDIMMs. Further, IDT's data buffer powers load-reduced DIMM (LRDIMM) applications to achieve top memory bandwidth (GB/s) on fully populated systems. The IDT chipset employs innovative features for best-in-class signal integrity that allow operation at highest possible speeds, even with heavy signal loads on high-density LRDIMMs.

“IDT provides an important part of Dell’s memory eco-system,” said Chad Fenner, director of Dell PowerEdge Server Solutions. “Dell has qualified 4RCD0224K register and 4DB0226K data buffer based RDIMM and LRDIMMs for our updated PowerEdge 13th generation servers based on Intel Xeon processor E5-2600 v4 product family. IDT has provided meaningful bandwidth improvements and solid support in optimizing LRDIMM applications for systems populated with capacities 768GB and higher.”

 “Micron has adopted IDT’s 4RCD0224K register and 4DB0226K data buffer for DDR4 LRDIMMs up to 128GB and RDIMMs up to 32GB for Intel Xeon processor E5-2600 v4 product family-based server systems,” said Matthias Buchner, Micron senior director of marketing, Compute & Networking Business Unit. “IDT has consistently provided competitive chipsets that enable Micron to deliver best in class products that meet the performance, power and capacity requirements of our Enterprise and Cloud customers.”

The latest chipset from IDT is verified to be fully compliant to the published JEDEC specifications. For more information about IDT’s DDR4 solutions, visit www.idt.com/go/DDR4.


About IDT

Integrated Device Technology, Inc. develops system-level solutions that optimize its customers' applications. IDT's market-leading products in RF, timing, wireless power transfer, serial switching, interfaces and sensing solutions are among the company's broad array of complete mixed-signal solutions for the communications, computing, consumer, automotive and industrial segments. Headquartered in San Jose, Calif., IDT has design, manufacturing, sales facilities and distribution partners throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol "IDTI." Additional information about IDT is accessible at www.IDT.com. Follow IDT on Facebook, LinkedIn, Twitter, YouTube and Google+.

IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. Intel and Xeon are registered trademarks of Intel Corporation in the United States and other countries. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.

Share this news on