Skip to main content

Renesas Launches Cloud-Based Environment to Accelerate Automotive AI Software Development and Evaluation

AI Workbench Empowers a Shift-Left Approach to Software Development and Decouples Software Design from Chip Availability

December 14, 2023

TOKYO, Japan ― Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, today launched a new cloud-based development environment aimed at streamlining the software design process for automotive AI engineers. The new platform, AI Workbench, is an integrated virtual development environment that empowers automotive AI engineers to design, simulate and fine-tune their automotive software - all within the cloud.

With this environment, engineers can immediately begin designing automotive software by leveraging Microsoft Azure services including Azure Compute, IaaS services, Microsoft Entra ID and Azure Security. Instead of installing tools on a PC or obtaining an evaluation board, they can perform tasks such as performance evaluation, debugging and verification using simulation tools online. This approach aligns with the "Shift-Left" approach, which enables software creation and testing earlier in the design cycle, even before the actual hardware becomes available. For example, it is possible to start developing AI-enabled application software to support ADAS (Advanced Driver Assistance System) and autonomous driving for the upcoming fifth-generation R-Car System on Chip (SoC) prior to the availability of hardware samples. This environment will serve as a unified development platform for designing and testing Renesas’ scalable automotive SoCs and microcontrollers (MCUs), regardless of product type or application.

“We are thrilled to introduce a cloud-based virtual development and AI model performance testing environment for automotive AI engineers in collaboration with Microsoft, a leading cloud technology provider," said Mandali Khalesi, Global VP, HPC AI and Cloud Technology at Renesas. “We are committed to improving the AI development environment through new features such as continuous monitoring and analysis of software usage.”

“Cloud-based development is a secure and cost-effective method to address the increasing complexities of today’s embedded projects. The collaboration between Renesas and Microsoft aims to tackle this challenge and accelerate the digital transformation of the automotive industry,” said Ulrich Homann, Corporate Vice President & Distinguished Architect, Cloud + AI, Microsoft. “With Renesas’ AI Workbench, developers can now efficiently build and test software for a myriad of applications using Renesas SoCs in a cloud-based environment powered by Azure."

The AI Workbench includes the following four functional blocks today. Renesas plans to enhance its offering in the future with additional features such as selected functionality or customization options tailored to support various development processes.

  1. Upgraded AI Compiler Toolchain
    Renesas will upgrade its SoC AI compiler toolchain with a novel “Hybrid Compiler (HyCo)” architecture and make it available through the AI Workbench. The new HyCo architecture developed in house and kernel libraries will allow engineers to unlock broader AI model and ONNX operator coverage, beyond the coverage of existing-third party hardware accelerator compilers available on Renesas SoC such as DSPs and NPUs.
     
  2. AI Model Performance Testing Environment
    Renesas will provide NNPerf, an online test environment for developers to evaluate the performance of AI models running on live Renesas SoCs with an updated hybrid AI compiler. Testing will run on real hardware in Renesas’ global device farm, without the need for evaluation boards. With the ability to batch code programs, perform real-time inference tests, and compare performance across different AI models, application engineers can estimate and make decisions on tradeoffs between models, memory footprints, latency and more.
     
  3. Software Development Environment
    Microsoft's code editor, Visual Studio Code (VSCode) and a software development kit (SDK) from Renesas are both available in the cloud. Using the tool suite, developers can launch their development environment in the cloud in a matter of minutes. Developers can customize their independent development environment and perform all design work using just a web browser on their PC.
     
  4. Software Evaluation/Verification Environment
    Renesas will also provide an environment for developers to test and verify their application software using the AI models defined in the AI model performance testing tool NNPerf. This includes simulators such as SILS (Software in the Loop Simulator), and HILS (Hardware in the Loop Simulator), allowing users to verify the operation designed for their specific AI application.

Availability

The AI Workbench will be available in January 2024 in limited preview. Renesas plans to expand availability of the AI Workbench from Q2 2024 and build similar environments for other major cloud services in the future. Additionally, Renesas will consider integrating tools provided by partners of the R-Car Consortium into the cloud environment for improved efficiency. More information about the AI Workbench is available at: renesas.com/ai-workbench.

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) empowers a safer, smarter and more sustainable future where technology helps make our lives easier. The leading global provider of microcontrollers, Renesas combines our expertise in embedded processing, analog, power and connectivity to deliver complete semiconductor solutions. These Winning Combinations accelerate time to market for automotive, industrial, infrastructure and IoT applications, enabling billions of connected, intelligent devices that enhance the way people work and live. Learn more at renesas.com. Follow us on LinkedIn, Facebook, X, YouTube, and Instagram.

(Remarks) All names of products or services mentioned in this press release are trademarks or registered trademarks of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

Share this news on