TOKYO, Japan ― Today, Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, introduced an update of its state-of-the-art R-Car V3H system-on-chip (SoC) to deliver significantly improved deep learning performance for smart camera applications, including driver and occupant monitoring systems (DMS / OMS), automotive front cameras, surround view, and auto parking for high-volume vehicles up to Level 2+. The updated SoC combines sensor fusion on the real-time domain with up to ASIL C metrics and an architecture optimized for smart computer vision. It offers OEMs and Tier 1s a high-performance, low-power solution that supports the latest NCAP 2020 requirements as well as the roadmap to NCAP 2025 3 Stars at competitive system costs.
Building on the state-of-the-art recognition technology introduced with the R-Car V3H in February 2018, which includes integrated IP for convolutional neural networks (CNN), the updated R-Car V3H delivers four times the performance for CNN processing compared to the earlier version and achieves up to overall 7.2 TOPS processing including all computer vision IPs while maintaining low power consumption levels.
The highly integrated SoC supports up to ASIL C metrics safety goals on the real-time domain, reducing the need for an external safety microcontroller (MCU) to manage sensor fusion and final decision actions. The R-Car V3H features a suite of proven IPs that support the perception stack, sensor fusion with radar and/or LiDAR, and ISP with up to eight MP cameras support, allowing OEMs and Tier 1s to achieve quicker time to market with lower bill of materials costs.
“The rising popularity of intelligent systems for applications, such as driver monitoring, park assist, driver recognition, and occupant sensing, is stoking higher demand for deep learning functions as automakers look for new ways to enable smart camera applications,” said Naoki Yoshida, Vice President of Automotive Digital Products Marketing Division at Renesas. “The updated SoC provides R-Car V3H customers a flexible, easy, and cost-effective path to higher computer vision performance for next-generation front camera systems, and we are excited to continue bringing cutting-edge innovation to our customers with our growing platform of open and scalable SoCs for ADAS and highly automated driving.”
Key Features of R-Car V3H SoC
- Delivers up to 7.2 TOPS, including 3.7 TOPS for CNN, with optimized performance-to-power balance
- Supports ASIL D development process for systematic capability for the full SoC
- Supports metric targets for ASIL B (sensor layer, application processors) and ASIL C (real-time domain) safety goals
- Full hardware and software compatibility with the currently mass-produced R-Car V3H SoC
- Integrates a full set of automotive peripherals including CAN, Ethernet AVB, and FlexRay
- Features a full set of video processing and image recognition IP for advanced sensing and recognition, including CNN-IP, Computer vision engine, Image-distortion-correction IPs, Stereovision, Classifier and Dense Optical Flow
The updated R-Car V3H joins Renesas’ expanding lineup of SoCs within the open and flexible Renesas autonomy platform, which offers OEMs and Tier 1s complete scalability from entry-level NCAP applications up to highly automated driving systems. Customers can also combine the R-Car V3H SoC with Renesas’ high-performance low-power RH850 MCU, integrated power management ICs, and power transistor devices to access the key components required for more complex safety compliant systems.
Availability
Mass production of the updated R-Car V3H is planned for first quarter of 2022. For more information, please visit: http://www.renesas.com/r-car-V3H
About Renesas Electronics Corporation
Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power, and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.
(Remarks). All names of products or services mentioned in this press release are trademarks or registered trademarks of their respective owners.
The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.