Skip to main content
Renesas Electronics Corporation

Renesas Blog

Renesas at Embeddd World 2022

Finally live again at Embedded World! Three inspiring days full of interesting conversations and exciting innovations

From 21-23 June, Renesas was one of the largest semiconductor manufacturers at Embedded World!

Motor Control System with Industrial Network and Functional Safety Blog

Future Proofing Industrial Automation for Tomorrow

In this blog, a simple and high-performance solution for motor control with industrial networking and functional safety (FuSa) features is introduced.

main blog image

RX Family Software – The Past and the Future - #4

The 32-bit RX family of MCUs’ software enables the development of applications with less or no coding. This blog focuses on the real-time OS for the RX family.

Enhance Touch and Gesture with AI Blog

Enhance Touch and Gesture with AI

The demand for enhanced intelligent touch and smart gesture recognition solutions is expanding with breakthrough applications across consumer and industrial segments.

Wi-Fi 6/6E Use Cases and Derived Wi-Fi AP Architectures

The 6GHz band promises economic potential and will enable new industry applications from entertainment to enterprise, industrial, and healthcare.

The Top 4 Reasons To Move Device Connectivity To Wi-Fi 6/6E TODAY!

The benefits of Wi-Fi 6 go beyond just speed. This blog offers four such benefits including greater bandwidth, resilience to congestion, reduced power consumption using TWT, and reduced latency.

The Potential Achilles Heel of Wi-Fi 6+6E Infrastructure Designs

Band filters between 5GHz and 6GHz may become a prohibiting factor for massive adoption and timely Wi-Fi 6+6E infrastructure designs. This blog covers the topic of band filters for Wi-Fi 6E in detail.

The Low-Power Advantage of Wi-Fi 6/6E: TWT Explained

We expect many of the consumer IT devices we use, which are battery-powered, to run for as long as possible. With Wi-Fi 6 there is a 4x capacity increase.

The Benefits of Having a Listening Radio in Wi-Fi 6+6E Tri-Band APs

In this blog, we will discuss the value and cost benefits of including a dedicated listening radio in a Wi-Fi AP, which can be extremely useful and beneficial.

RX72M offers effortless evaluation of stepper motor control with EtherCAT

RX72M Offers Effortless Evaluation of Stepper Motor Control with EtherCAT

In this blog, we introduce using the RX72M 32-bit microcontroller for resolver stepper motor control via EtherCAT communications.