Easy-to-Start Automotive MCU Accelerates the Development Cycle
Introducing the Easy-to-Start automotive microcontroller series that are easy to use, easy to develop and easy to access for automotive, industrial and consumer applications.
Introducing the Easy-to-Start automotive microcontroller series that are easy to use, easy to develop and easy to access for automotive, industrial and consumer applications.
Learn about the importance of air quality to our health and the benefits of being able to monitor air quality, regardless of location, with Renesas’ ZMOD4510 outdoor air quality sensor.
Introducing the real-time OS project creation function, which is an essential function for those who are using an embedded real-time OS.
Ethernet TSN Switch IP Core is a high-quality IP core that has passed the conformance test provided by Spirent Communications; watch the video of the IP core evaluated by FPGA using Spirent Automotive C1.
The RX23E-A, which integrates an MCU and high-precision Analog Front End on a single chip, is ideal for realizing integrated sensing and signal conditioning of a digital load cell in the same housing.
With an ASIC solution, all the condition monitoring circuitry can be placed on the same chip with all the required electronics for the core function of the product.
In this blog, we give a brief background summary of PCIe, what its potential PCIe use cases are and what needs to be looked at to smoothen the adaption path of PCIe in future automotive applications.
The RX family of 32-bit MCUs offers evaluation kits with Azure Certified Device certification, sample code and IDE for deploying Azure RTOS. These enable easy connection to Azure IoT Hub.
H8SをFPGAに組み込んだ実装例を元にFPGAマイコンをご紹介します。
This blog introduces the xEV market status in Europe, one of the most active areas, and our promotional activities.