Skip to main content

Trigonometry

Trigonometry

This library provides trigonometry functions, carrying out sin, cos and tan calculations.

sin

Description
Calculates the sine of an angle (in radians).
Syntax
sin(rad)
Parameters
rad: The angle in radians (float)
Returns
The sine of the angle (double)

cos

Description
Calculates the cosine of an angle (in radians).
Syntax
cos(rad)
Parameters
rad: The angle in radians (float)
Returns
The cosine of the angle (double)

tan

Description
Calculates the tangent of an angle (in radians).
Syntax
tan(rad)
Parameters
rad: The angle in radians (float)
Returns
The tangent of the angle (double)

Sample Program


#include <Arduino.h>
void setup(){
    Serial.begin(9600);
}
    
void loop(){
        // print labels 
    Serial.print("RAD");       // prints a label
    Serial.print("\t");        // prints a tab
    
    Serial.print("SIN");  
    Serial.print("\t");      
    
    Serial.print("COS"); 
    Serial.print("\t");   
    
    Serial.print("TAN");
    Serial.print("\t");
    Serial.println("");
        
    for(float x=0; x< PI; x+=0.01){    // only part of the ASCII chart, change to suit
    
    // print it out in many formats:
        Serial.print(x);       // print as an ASCII-encoded decimal - same as "DEC"
        Serial.print("\t");    // prints a tab
    
        Serial.print(sin(x));  // print as an ASCII-encoded decimal
        Serial.print("\t");    // prints a tab
    
        Serial.print(cos(x));  // print as an ASCII-encoded hexadecimal
        Serial.print("\t");    // prints a tab
    
        Serial.print(tan(x));  // print as an ASCII-encoded octal
        Serial.print("\t");    // prints a tab
    
        Serial.println("");      // prints another carriage return
        delay(100);            // delay 100 milliseconds
    }
    
}