Skip to main content

Utility

Utility

Introducing the specific libraries for the GR-KAEDE board.

system_reboot

Description
Reset
Syntax
void system_reboot(mode)
Parameters
mode: Specify the mode of reset (REBOOT_USERAPP or REBOOT_FIRMWARE)
Returns
None
Note
Specify #include <reboot.h> for use

Sample Program

This example shows a reset every 1 second.


#include <Arduino.h>
#include <reboot.h>
void setup()
{
    pinMode(PIN_LED0, OUTPUT);
    digitalWrite(PIN_LED0, HIGH);
    
    delay(1000);
    
    system_reboot(REBOOT_USERAPP);
//    system_reboot(REBOOT_FIRMWARE);
    
}
    
void loop()
{
}