Skip to main content

Harsh Environment Products

As a major supplier to the military and aerospace industries, Renesas' product development methodologies reflect experience designing products to meet the highest standards for reliability and performance in challenging environments.

Manufacturing & Test Information

As a major supplier to the military and aerospace industries, Renesas' product development methodologies reflect experience designing products to meet the highest standards for reliability and performance in challenging environments.

The low dose rate ionizing dose response of semiconductors has become a key issue in space applications. Renesas is addressing this market by wafer-by-wafer low dose rate acceptance testing as a complement to current high dose rate acceptance testing.

Renesas is one of only a few RHA Defense Logistics Agency (Land and Maritime) QML suppliers. All of Renesas' radiation hardened SMD products are MIL-PRF-38535/QML compliant and are 100% burned in.

Categories

Harsh Environment A/D Converters
Low-power A/D converter for FemtoCharge™ technology on a standard CMOS process
Harsh Environment Amplifiers
Amplifiers to meet the highest reliability and performance standards for harsh environments
Harsh Environment Comparators
Monolithic, quad, precision comparators for accurate, high-speed, signal level detection
Harsh Environment Data Communications ICs
Receivers, line drivers and encoder-decoders for data communications applications
Harsh Environment Digital Controlled Potentiometers (DCPs)
Single, dual and quad DCPs implemented with a combo of resistor elements and CMOS switches
Harsh Environment Half, Full Bridge and Three Phase FET Drivers
Drivers optimized for PWM motor control and UPS system applications
Harsh Environment Isolated PWM Switching Controllers
Single-ended, current mode controllers for boost, flyback and isolated output configurations
Harsh Environment Microprocessors and Peripherals
Microprocessors and peripherals for space and harsh environment applications
Harsh Environment RS-485/RS-422 Serial Interface
ESD protected transmitter/receiver devices that meet balanced communication standards
Harsh Environment SAR A/D Converters
12-bit analog-to-digital converters that are qualified to QML Class Q military standards
Harsh Environment Sample and Hold Converters
Sample and hold amplifiers for use in precision, high-speed data acquisition systems
Harsh Environment Switches/MUXs/Crosspoints
Devices that offer excellent performance across a wide input voltage range
Harsh Environment Transistor Arrays
Devices that consist of 5 dielectrically isolated transistors on a common monolithic substrate

Product Selector: Harsh Environment Products

Explore our catalog of products through our parametric product selector tool. Compare specifications across various parameters to find the right part for your design.

Product Selector

Documentation

Type Title Date
Brochure PDF 5.02 MB
Application Note PDF 341 KB
2 items

Videos & Training

Are Your ICs Ready for the Real Space Environment?

Over the past 19 years, the space industry has placed a higher value on understanding the effects that long-term, low dose radiation can have on ICs. Intersil's radiation testing specialist Nick van Vonno discusses why this shift has occurred and what we are doing to address this change.

Transcript

There are many different types of radiation, and indeed Intersil addresses two of these. Intersil addresses total dose testing which is basically gamma rays. Okay, and at both high and low dose rate, as we'll get into later. Intersil also addresses single event effects of a fairly broad range, and those are typically addressed by heavy ion testing.

Low dose rate testing, you have to contrast this really in order to understand this. You have to look historically at how total dose testing which is done with gamma rays, how that's been performed. Historically this has been performed at what we call high dose rate, and typically to put this in some numbers, that would run somewhere in the range of 50rad to 300rad/s.

Low dose rate, on the other hand, is a much, much slower dose rate. The generally accepted number, and the one we perform our work in, is 0.01rad/s. You see how far that's away from 300rad a second. And that can also be expressed as 10mrad/s if you'd like.

Now why are we goofing with that? And the answer is that the low dose rate is what happens in space. Dose rates in space are almost uniformly low to the order of 10mrad/s. Low dose rate radiation testing has been a, let's call it a hot topic in silicon advanced research since about 1992, okay? In 1992, some researchers out at Mich research came up with a very unusual finding which showed that certain parts that looked very good at high dose rate degrade with amazing rapidity, orders and orders of magnitude, worse at low dose rate. And so, that was not a fully intuitive result, and indeed it had to be repeated, and in the intervening 19 years there is a very large amount of work that's been done on low dose rate effects. And, as we've learned about how different parts react in low dose rate, we've, as an industry, we've swung over more towards a low dose rate testing emphasis rather than a high dose rate testing emphasis.

Tools & Resources