Overview
Description
The real-time OS aware debugging presented herein supports task-level debugging of real-time OS applications in the Integrated Development Environment High-performance Embedded Workshop. This function comes standard with High-performance Embedded Workshop. There is no need to rebuild the real-time OS, nor will overhead be incurred. (Debug patches, etc. are not necessary.)
Features
- Object status reference (OS object window)
- Graphical display of task execution history (task trace window)
- Graphical display of task execution time (task analyze window)
- Functions for the E100 emulator
- Learn more
Release Information
Target Devices
Additional Details
Functions
- Object status reference (OS object window)

- Allows you to inspect the execution status of objects such as tasks and semaphores
- RAM monitor supported
- Capable of a mixed display of multiple objects such as task priority and event flag value
When using Renesas real-time OSs, you can make use of extended debugger options that permit more detailed object status references (real-time OS debugger [Debugging Extension] task window, etc. and MR window of the PC7501 emulator, etc.). These windows include the items normally displayed in the OS object window. (The relationship between these windows and the OS object window is similar to the relationship between a watch window and local window.)
- Graphical display of task execution history (task trace window)
- Execution history display making use of trace data

- Graphical display of task execution time (task analyze window)
- Execution time and CPU occupancy rate display making use of trace data

- Functions for the E100 emulator
- Real-time profile (shows the CPU occupancy rate over a long time without interruption)
- Task specification for each condition (break, performance, trace and trace filter)
- Currently executed task display in the status bar
- Task execution history display in text form (execution history display making use of trace data)
- Task stack coverage (graphical display of the task stack used)
- Memory protection (illegal accesses to the task stack and OS area detected)
- Step execution aiming at a specific task
- Dispatch detection and break



Refer to the help file of the E100 emulator for more information about the functionality.
Function Relationship
[Real-time OS] Table 1
Function | HI7200/MP, HI7750/4, HI7700/4, HI7000/4 |
RI600/4 | M3T-MR30/4, M3T-MR30 |
HI1000/4 | MR8C/4, Smalight OS |
---|---|---|---|---|---|
OS object | ✔ | ✔ | ✔ | ✔ | ✔ |
Task trace | ✔ | ✔ | ✔ | ✔ | ✔ |
Task analyze | ✔ | ✔ | ✔ | ✔ | ✔ |
OS trace | - | ✔ | ✔ | - | - |
OS analyze | - | ✔ | ✔ | - | - |
Task step | - | ✔ | ✔ | ✔ | ✔ |
Currently executed task display | - | ✔ | ✔ | ✔ | ✔ |
Execution history display | - | ✔ | ✔ | ✔ | ✔ |
Realtime profile | - | ✔ | ✔ | ✔ | ✔ |
Task specification | - | ✔ | ✔ | ✔ | ✔ |
Stack coverage | - | ✔ | ✔ | - | ✔ |
Memory protection | - | ✔ | ✔ |
- |
✔ |
Detection of dispatch | - | ✔ | ✔ | ✔ | ✔ |
[Real-time OS] Table 2
Function | ThreaX, TOPPERS/JSP | embOS | NORTi, uC/OSⅡ, uT-Kernel | osCAN, TOPPERS/ASP | RTA-OSEK |
---|---|---|---|---|---|
OS object | ✔ | ✔ | ✔ | ✔ | - |
Task trace | ✔ | ✔ | ✔ | ✔ | ✔ |
Task analyze | ✔ | ✔ | ✔ | ✔ | ✔ |
OS trace | - | - | - | - | - |
OS analyze | - | - | - | - | - |
Task step | - | - | - | - | - |
Currently executed task display | - | ✔ | ✔ | ✔ | - |
Execution history display | - | - | ✔ | ✔ | - |
Realtime profile | - | - | ✔ | ✔ | - |
Task specification | - | - | ✔ | ✔ | - |
Stack coverage | - | - | - | ✔ | - |
Memory protection |
- |
- |
- |
- |
- |
Detection of dispatch | - | - | - | - | - |
[Debugger]
Function | Simulator | E1 | E20 | E10A-USB | E8a | E100 | E200F |
---|---|---|---|---|---|---|---|
OS object | ✔ | ✔ | ✔ (RAM monitor supported2) |
✔ | ✔ | ✔ (RAM monitor supported) |
✔ |
Task trace | ✔ | ✔5 | ✔5 (Large capacity2) |
✔1 | - | ✔ (Large capacity) |
✔ |
Task analyze | ✔ | ✔5 | ✔5 (Large capacity2) |
✔1 | - | ✔ (Large capacity) |
✔ |
OS trace | ✔3 | - | - | - | - | ✔4 | - |
OS analyze | ✔3 | - | - | - | - | ✔4 | - |
Task step | - | ✔ | ✔ | - | - | ✔ | - |
Currently executed task display | - | ✔ | ✔ | - | - | ✔ | - |
Execution history display | - | - | - | - | - | ✔ | - |
Real-time profile | - | - | - | - | - | ✔ | - |
Task specification | - | - | - | - | - | ✔ | - |
Stack coverage | - | - | - | - | - | ✔ | - |
Memory protection | - | - | - | - | - | ✔ | - |
Detection of dispatch | - | - | - | - | - | ✔ | - |
- 1. Use 36-pin or 38-pin cable. (14-pin cable can not use.) Time is not displayed. (except for SH2A-DUAL)
- 2. Use 38-pin cable. (14-pin cable can not use.)
- 3. apply only when Simulator debugger for RX family V.1.02.00 or later is in use.
- 4. apply only when M16C R8C E100 Emulator Software V.1.03 Release 00 or later and M16C/60 or M16C/50 series are in use.
- 5. apply only when E1 or E20 emulator debugger for RX family is in use.
Operating Environment
- Host machine
Refer to Operating Environments of Products. - Corresponding integrated development environment High-performance Embedded Workshop
V.4.09.00 or later
Corresponding Real-Time OS
Real-time OS | Microcontrollers | |
---|---|---|
Renesas HI7200/MP | V.1.00 Release 03 or later | SH2A-DUAL |
Renesas HI7750/4 | V.2.02 Release 04 or later | SH-4, SH-4A |
Renesas HI7700/4 | V.2.03 Release02 or later | SH4AL-DSP, SH-3, SH3-DSP |
Renesas HI7000/4 | V.2.02 Release 04 or later | SH-2, SH2-DSP, SH-2A, SH-1 |
Renesas RI600/4 | V.1.00 Release 00 or later | RX Family |
Renesas M3T-MR30/4 | V.4.00 Release 00 or later | M16C/60, M16C/50, M16C/30, M16C/20, M16C/10, M16C/Tiny Series |
R8C Family | ||
Renesas M3T-MR30 | V.3.30 Release 2 or later | M16C/60, M16C/50, M16C/30,M16C/20, M16C/10, M16C/Tiny Series |
Renesas MR8C/4 | V.1.00 Release 00 or later | R8C Family |
Renesas HI1000/4 | v1.05 Release01 or later | H8SX Family |
H8S Family | ||
Smalight OS made by Maxell System Tech Co., Ltd. | V3.10 or later | SH-2, SH-2A |
RX Family | ||
M16C/Tiny, M16C/30 and M16C/60 Series | ||
R8C Family | ||
H8SX Family | ||
H8S Family | ||
H8 Family | ||
ThreadX made by Express Logic, Inc. | G5.1.5.0 | SH-2A |
NORTi made by MiSPO Co., Ltd. | Version4 Release 1.20 | SH-4A, SH-2A |
Version4 Release 4.3G | RX Family | |
Version4 Release 1.14 | H8SX Family | |
H8S Family | ||
osCAN made by Vector Informatik GmbH. | Version 3.05 | M16C/60, M16C/Tiny Series |
RTA-OSEK made by ETAS Co., Ltd. | Version 4.0.0 | SH-2A |
uC/OS-II made by Micrium Inc. | V.2.86 (AN-Renesas-SH7201) | SH-2A |
V.2.89 | RX Family | |
V2.83 (AN-1662) | M16C/60 Series | |
V.2.86 (AN-Renesas-H8S2215R, AN-Renesas-H8S2472, AN-Renesas-H8SX1664) | H8SX Family | |
H8S Family | ||
embOS made by Microcontroller GmbH & Co. KG | Version 3.80g | SH-2A |
Version 3.82b | RX Family | |
CMX-RTX made by CMX Systems Inc. | Version 5.30 | RX Family |
TRON Forum uT-Kernel | v1.00.00 | M16C/62P Group |
TOPPERS Project TOPPERS/ASP | Release 1.3.1 | SH-2A |
Release 1.3.2 | M16C/60 Series | |
TOPPERS Project TOPPERS/JSP | Release 1.4.3 | H8/3048 Group |
H8S/2350 Group |
Corresponding Debuggers
Debugger | Supported microcontrollers | Supported debugger version |
---|---|---|
Simulator debugger | SuperH Family | V.9.08.00 or later |
RX Family | V.1.00.00 ot later | |
H8SX, H8S and H8 Family | V.5.07.00 or later | |
E1 emulator debugger | RX Family, R8C Family | V.1.00 Release 00 or later |
E20 emulator debugger | RX Family, R8C Family | V.1.00 Release 00 or later |
E10A-USB emulatordebugger | SH-2A, SH-4A, SH4AL-DSP, H8SX Family, | V.3.00 Release 00 or later |
H8S Family | ||
SH2A-DUAL, SH4A-MULTI | V.2.00 Release 00 | |
E8a emulator debugger | M16C Family, R8C Family, H8 Family | V.1.02 Release 00 or later |
E100 emulator debugger | RX Family, M16C Family, R8C Family, | V.1.00 Release00 or later |
H8SX Family | ||
E200F emulator debugger | SH-2A | V.3.00 Release 00 |
*. Please refer to the Emulator pages linked above to get to know the detailed supported MCUs.
Corresponding Compilers
- C/C++ Compiler Package for SuperH Family V.9.02 Release 00 or later
- C/C++ Compiler Package for RX Family V.1.00 Release 00 or later
- C Compiler Package for M16C Series and R8C Family [M3T-NC30WA] V.5.43 Release 00 or later
- C/C++ Compiler Package for H8SX, H8S, H8 Family V.6.02 Release 00 or later
*TRON Forum holds the copyright on the uITRON Specification and the uT-Kernel specifications.
*The OSEK/VDX steering committee holds the copyright on the OSEK/VDX specifications.
*TOPPERS is a registered trademark of TOPPERS Project.
*OSEK is a registered trademark of Siemens AG.
*ThreadX is a registered trademark of Express Logic, Inc.
*NORTi is a registered trademark of MiSPO Co., Ltd.
*osCAN is a registered trademark of Vector Informatik GmbH.
*RTA-OSEK is a registered trademark of LiveDevices Co., Ltd.
*Smalight is a registered trademark of Maxell System Tech Co., Ltd.
*uC/OS-II is a trademark of Micrium, Inc.
*embOS is a registered trademark of SEGGER Microcontroller GmbH & Co. KG.
*CMX-RTX is a trademark of CMX Systems Inc.
*The other system names and product names referred to in this document are trademarks or registered trademarks of the respective proprietary companies.
*TRON, ITRON, uITRON, uT-Kernel and OSEK/VDX do not refer to any specific product or products.
Design Support
High-performance Embedded Workshop Real-Time OS Aware Debugging Information for Users