DRP-AI Handles both AI Inference and Image Processing Functions, Eliminating  External ISP Requirements and Enabling More Cost-Efficient Vision AI Implementations

May 19, 2021

TOKYO, Japan ― Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, today announced the expansion of its RZ/V Series of microprocessors (MPUs) with the new RZ/V2L MPUs designed for entry-level AI-enabled applications. As part of the RZ/V Series, the new MPUs incorporate Renesas’ exclusive AI accelerator – the DRP-AI (Dynamically Reconfigurable Processor) – to make embedded AI easier and more power efficient. The new RZ/V2L shares several features with its predecessor, the RZ/V2M, such as high-precision AI inference capabilities combined with top-class power efficiency. It also includes optimizations such as tailoring the DRP-AI operating frequency and memory interface for an entry-level MPU.

The DRP-AI provides both real-time AI inference and image processing functions with the capabilities essential for camera support such as color correction and noise reduction. This enables customers to develop AI-based vision applications, such as point-of-sale (POS) terminals and robot vacuum cleaners, without requiring an external image signal processor (ISP). In addition, the RZ/V2L’s excellent power efficiency eliminates the need for heat dissipation measures such as heat sinks or cooling fans. Now AI can be implemented cost efficiently not only in surveillance cameras and industrial equipment, but also in a wide range of applications including home appliances and consumer electronics.

The RZ/V2L is also package- and pin-compatible with the existing RZ/G2L general-purpose MPUs. This allows RZ/G2L users to easily upgrade to the RZ/V2L for additional AI functions without needing to modify the system configuration, keeping migration costs low.

“One of the most important trends in the electronics industry today is the incorporation of AI into embedded devices – especially AI for interpreting sensor data, such as images,” said Jeff Bier, General Chairman of the Embedded Vision Summit and Founder of the Edge AI and Vision Alliance. “Innovative processors like the RZ/V2L are key for enabling perceptual AI to be incorporated into a wide range of cost- and power-constrained IoT devices.”

“Our new entry-level AI accelerator products provide customers with the flexibility to select the most suitable product from a wide range of MPU offerings,” said Hiroto Nitta, Senior Vice President and Head of SoC Business in the IoT and Infrastructure Business Unit at Renesas. “These AI-optimized solutions will expand the use of embedded AI to a wider range of applications such as home appliances and consumer electronics, as customers can now implement AI capability with lower system costs.”

As part of the the RZ/V2L development environment, Renesas offers a complimentary DRP-AI Translator, a tool that automatically converts AI models into an executable format. The input format is the industry-standard Open Neural Network Exchange (ONNX). Developers can leverage the DRP-AI while using the tools they are accustomed to, allowing them to immediately start using the RZ/V2L to evaluate AI models based on proven learning data.

Key Features of the RZ/V2L MPUs

  • 64-bit Arm® Cortex®-A55 (1.2 GHz, dual or single core) and Cortex-M33
  • DRP-AI (1 TOPS/W class) AI accelerator capable of running the Tiny YOLOv2 program at 28 frames per second (fps)
  • Simple ISP functions required for machine vision are provided in the DRP library (supports up to full HD)
  • 16-bit, single-channel DDR memory interface
  • 3-D graphics functions (Arm Mali™-G31 GPU)
  • Video codec (H.264)
  • CMOS sensor interfaces (MIPI-CSI and Parallel) for camera input
  • Display interfaces (MIPI-DSI and Parallel)
  • Memory with error checking and correction (ECC)
  • Verified Linux Package (VLP) based on Civil Infrastructure Platform Linux, an industrial-grade Linux implementation, available
  • Available in 15 mm square or 21 mm square BGA packages that are pin-compatible with the RZ/G2L

As part of a series of comprehensive solutions for assisting rapid development called "Winning combinations," Renesas offers solutions using mutually compatible devices that work together seamlessly for reduced design risk. RZ/V2L evaluation boards are provided as "SMARC (Smart Mobility ARChitecture) SoM (System-on-Module) Solution” to enable quick validation for different applications. "SMARC Solution" is also available for existing RZ/G2 MPUs. These reference designs provide an optimized circuit diagram and board layout, and include a power supply circuit and timing tree. Furthermore, a power management IC (PMIC) optimized for the RZ/V2L is currently in development, and solutions incorporating the RZ/V2L and new PMIC are expected to become available in the second half of 2021. "Winning Combinations" are engineering-vetted system architectural solutions that combine Renesas' expertise in analog, power, and embedded computing to help customers get to market faster.

Availability

Sample shipments of the RZ/V2L start today, and mass production is scheduled to begin in December 2021. For more information on the RZ/V2L MPUs, please visit: https://www.renesas.com/rzv2l. The SMARC SoM Solution is available now.

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power, and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.

(Remarks). Arm, Arm Cortex and Arm Mali are trademarks or registered trademarks of Arm Limited in the EU and other countries. All names of products or services mentioned in this press release are trademarks or registered trademarks of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

Share this news on