Environmental Activities
Environmental Initiatives | Environmental Protection Goals | Climate Change Initiatives | Conserving Water | Waste Reduction Efforts | Chemical Substance Use | Eco-Product Initiatives | Eco-Communication Initiatives | Biodiversity Conservation Activities | Environmental Data and Third-Party Verification
Eco-Product Initiatives
Renesas is committed to eco-product initiatives and creating environmentally-conscious products and solutions that contribute to energy conservation and efficiency.
Creating Environmentally-Conscious Products
In order to create environmentally-conscious products, it is important to reduce the environmental impact at all stages of the product lifecycle, from development, procurement, manufacturing, use and disposal. Our eco-products are the results of product environmental assessments (Note 1) which evaluate the total environmental impact reduction measures (Product Stewardship). During these product environment assessments, our products are tested and evaluated at two stages: at the development stage and before mass production.
In addition, we have made product environmental assessments as part of the requirements in new product development, and we are working to raise internal awareness of the importance of product stewardship through training for project leaders and future leaders involved in new product development.
*1: Currently, the product environmental assessment is conducted only for former Renesas products, but we are considering expanding the scope in the future.
Eco-Product initiatives at each stage

Environmental Assessments of Products
We create environmentally-conscious products by incorporating product environmental assessments into the product development and design flow, to evaluate the degree of improvement in environmental load. In this assessment, we make comparisons between our target products with indexed previous generations of the products (Note 2) based on eight criteria, including weight reduction, product safety, and whether they are energy saving.
Eight Criteria for Product Environmental Assessment
Safety evaluation | Resource and energy-saving evaluation |
---|---|
|
|
The outcome of the assessment is determined by the design department developing the product as well as the Environmental Promotion Department at head office of Renesas as a third-party assessor. If the outcome determines that any of the three categories below applies, the sale of the product is prohibited in principle.
- If a prohibited material is used in the product or in the manufacturing process
- If a new material used in the product or in the manufacturing process is not SDS (Note 2) registered
- If the preliminary examination of any new materials used in the manufacturing process has not been conducted
In addition, if the environmental performance of a product has not improved in comparison to the indexed product, the design department must consider making improvements to the product or decide whether the development should continue.
The steady promotion of the environmental assessment increases the safety and trust of Renesas’ semiconductor products, as well as to further improve the environmental performance of the products themselves. This will ultimately lead to reducing the environmental impact for the final customers using our finished products.

Note 2: Previous generation refers to indexed products that are one generation prior but have almost the same purpose, function and performance as the new product. However, if there are no previous generations of a product, the new product itself is considered as the index product.
Note 3: Safety Data Sheet (SDS) refers to the information document provided by supplies on the properties of chemical substances and the handling of materials that contain hazardous substances that may be dangerous or harmful.

Renesas Green Devices
In order to promote research and development (R&D) and design of products that support the creation of environmentally-conscious products based on the Environmental Action Guidelines in all stages of the product life cycle, products that greatly contribute to the reduction of environmental impact are certified as "Renesas Green Devices.”
Green Devices are certified products that have completed the development stage but have not yet been mass produced. The certification process is basically as follows: Firstly, based on the results of the product environmental assessments, we confirm whether the environmental performance of the target product is more superior to the indexed product in the three categories of resources (mass), energy (energy consumption) and chemical substances (quantity of substances used by Renesas that are subject to reduced usage). Secondly, if the target product is determined to be superior to the indexed product and the improvement rate is over 10%, the product is certified as “Renesas Green Devices.” In fiscal year 2023, Renesas Green Devices accounted for 96% (Note 4) of new product development, and approximately 60% of total sales (Note 5), including affiliated products.
Evaluation criteria | Comparison between indexed product and new product | Renesas Green Devices | |
---|---|---|---|
Resource-saving evaluation |
| 10% or more reduction | 96% Percentage of Renesas Green Devices in new product development (Note 4) |
Energy-saving evaluation |
| ||
Chemical substance content evaluation |
|
Note 4: Percentage of Renesas Green Devices among the number of former Renesas products developed in FY2023.
Note 5: Percentage of Renesas Green Devices (former Renesas products developed and mass-produced in FY2023 and their affiliated products) to sales of former Renesas products in FY2023.
Lead-free products within Renesas Green Devices
Renesas’ semiconductor products are used in many products that are marketed around the world. To comply with environmental laws and regulations related to our products, we research the laws and regulations of major countries, apply the information in our group products, and communicate with our customers on the chemical substance content in a timely manner. In addition, Renesas is actively working to reduce the use of lead-free products, as the demand for semiconductor products and electronic devices continues to grow.
Proportion of number of lead-free products developed | |
---|---|
New development of Renesas Green Device | 90% |
here to learn about our compliance with environmental laws and regulations.
Click here to learn about our lead-free initiatives.
Renesas Super Green Devices
Among Renesas Green Devices, products with superior performance are certified as "super green devices."
Evaluation criteria | Comparison between indexed product and new product | |
---|---|---|
Resource-saving evaluation |
| 50% or more reduction |
Energy-saving evaluation |
| |
Chemical substance content evaluation |
|
Examples of Renesas Green Devices and Super Green Devices
Products certified as “Renesas Green Devices” and “Renesas Super Green Devices” for having superior environmental performance among hundreds of products developed annually at Renesas are registered in a database. Some of the products that can be publicly disclosed are uploaded onto the Renesas website. Going forward, Renesas will continue to promote the creation of environmentally-conscious products by recognizing green device certified products in award systems and more.
Introduction of Renesas Green Devices and Super Green Devices (Products developed in 2023)
Excerpt from products that can be publicly disclosed
Product name | Type | Application | Feature |
---|---|---|---|
R7F102G4E3CNP R7F102G4C3CNP R7F102G4E2DNP R7F102G4C2DNP | MCU with low current consumption and capacitive touch channel | RL78 general-purpose microcontroller for home appliances, consumer equipment, and industrial equipment | In addition to the industry's lowest level of low current consumption, it is equipped with a wide variety of capacitive touch channels. New generation RL78 general-purpose microcontroller lineup with various 16-48 pin packages and 32KB to 64KB flash memory Learn more about RL78/G22 |
R7F123FMG5AFB-C R7F123FLG5AFB-C R7F123FGG5AFB-C R7F123FBG4ANP-C | 16-bit MCU for actuator/sensor control | Automotive | Product for realizing next-generation smart actuators & sensors and low-end body ECUs that require high reliability Learn more about RL78/F23 |
R7F124FBJ4ANP-C | 16-bit MCU for actuator/sensor control | Automotive | Product for realizing next-generation smart actuators & sensors and low-end body ECUs that require high reliability Learn more about RL78/F24 |
R7FA8M1A*ECFB R7FA8T1A*ECFB R7FA8M1A*ECFC R7FA8D1**ECFC R7FA8T1A*ECFC R7FA8M1A*ECFP R7FA8T1A*ECFP | RA Family Arm® Cortex®-M based 32Bit MCU | General industry/consumer use | Reduces overall system power consumption with multiple low-power modes, power domain separation, low-voltage operation, fast wake-up, low operating and standby current combinations, and more Learn more about RA4M3 |
R7FA6E2BB2CBB R7FA6E2BB2CBC R7FA6E2B92CBB R7FA6E2B92CBC | RA Family Arm® Cortex®-M based 32Bit MCU | General-purpose microcontroller with TrustZone® for general industry and consumer use | Based on a 200 MHz Arm® Cortex®-M33 core with TrustZone, it pursues a balance between cost and functionality, achieving best-in-class performance as an entry-line microcontroller. Learn more about RA6E2 |
R7F101G6G4CSP R7F101G6E4CSP R7F101G6G3CSP R7F101G6E3CSP R7F101G6G2DSP R7F101G6E2DSP | Low power 8/16 bit MCU | For home appliances, consumer equipment, and industrial equipment | A microcontroller with the highest level of processing performance among the RL78 family MCUs, equipped with a CPU operation with a maximum operating frequency of 48MHz and a flexible application accelerator (FAA). Additionally, it has enhanced analog functionality and a rich set of timers, making it suitable for motor control, power supply, and lighting applications. FAA is a coprocessor dedicated to calculations and can operate independently of the CPU, achieving higher processing power. Learn more about RL78/G24 |
R9A09G057H48GBG | MCU equipped with Renesas' proprietary AI accelerator (DRP-AI3), quad Arm® Cortex®-A55 (1.8GHz) Linux processor, and dual Cortex®-R8 (800MHz) real-time processors | Industrial (autonomous robots, factory automation, etc.) | In addition to the AI accelerator, it is equipped with another dynamic reconfiguration processor (DRP), which can accelerate image processing such as OpenCV and dynamics calculations required for robot applications. Learn more about RZ/V2H |
Environmental contribution of Renesas Green Devices
Renesas aims to make people's lives easier through our products and solutions, and contribute to building a future that creates a better world. In a world where everything around us is intelligent and interconnected, advanced computing performance is a must. At the same time, the demand for energy efficiency and robust safety and security will continue to increase. By providing our customers Renesas Green Devices that meet these growing demands, we can foster a greener and more sustainable society.
Renesas Green Devices not only reduce the use of resources, energy, and prohibited chemical substances in the product itself, but also contribute to improving the energy efficiency of customers' systems by incorporating our solutions into their products. We also play a role in increasing energy efficiency of society, as our customers' products are used across many applications.
Renesas' core business is to foster a sustainable society by providing products and solutions in mission-critical business fields that form the basis of our society, such as automobiles, factory automation (FA), communication infrastructure, and medical and healthcare. Specifically, we will focus on developing low-power products with minimum environmental impact and products and solutions that make people's lives safer and more secure, and advancing research and development for innovation that supports them.
Renesas Green Device solutions (Note 6) that contribute to a sustainable society
Renesas Green Devices | ||
---|---|---|
Mission-critical business areas (Automotive, FA, communication infrastructure, medical, healthcare, etc.) | Other business fields | |
Clean Transportation | Energy Efficiency | Other business solutions |
|
|
|
Sales ratio of Renesas Green Devices by solution (Note 7)
In FY2023, 67% of Renesas' green device sales was for mission-critical business areas (green bond eligible solutions), of which 38% was for smart vehicle solutions and electric vehicles, and 29% for social infrastructure such as data centers and cellular.

Note 6: Solutions are classified according to the green eligibility category of the green bond framework effective in November 2021.
Note 7: Renesas' green devices (former Renesas products and related products that were developed and began mass production in FY2023) are classified as green bond eligible solutions, and the ratio for each solution is calculated using the sales of green device products as the denominator. The proportion of products that could not be classified was approximately 33%.
here.
Read more about Renesas’ products and solutions that contribute to a sustainable society through customers’ systemsProduct Environmental Quality in Supply Chain
We believe that it is necessary for the entire supply chain to manage chemical substances contained in products throughout the process, from the selection of materials during development and design, to the prevention of pollution in the manufacturing process. For this reason, we ask suppliers to submit certificates and analysis data to confirm that prohibited substances are not used, and they adhere to such practices in supplier audits. Distributors are requested to manage the chemical substances contained in the packaging materials they use. On the other hand, we also provide our customers with information on chemical substances contained in products and analysis data on prohibited substances according to the RoHS Directive to ensure that our products can be used safely. In addition, we share with customers our systems for managing chemical substances and the progress of our environmental activities.
here to learn about our environmentally-conscious supply chain initiatives.
Click here to learn about our green procurement.
Click here to learn about our environmental compliance.

Contributing to SDGs
Renesas’ efforts in Eco-Product Initiatives contributes to these Sustainable Development Goals targets:

12.4 By 2020, achieve the environmentally-sound management of chemicals and all wastes throughout their life cycle, in accordance with agreed international frameworks, and significantly reduce their release to air, water and soil in order to minimize their adverse impacts on human health and the environment
Environmental Activities
Environmental Initiatives | Environmental Protection Goals | Climate Change Initiatives | Conserving Water | Waste Reduction Efforts | Chemical Substance Use | Eco-Product Initiatives | Eco-Communication Initiatives | Biodiversity Conservation Activities | Environmental Data and Third-Party Verification