Skip to main content

Renesas Blog

Main blog image

Recommending the H8S Family Microcontroller IP to Users Looking For H8/3048-like IP

We strongly recommend using the H8S IP if you are looking for IP for an H8/300H microcontroller such as one from the H8/3048F or H8/3052F group.

The Importance of Reference Documentation for Consumers and Engineers

The Importance of Reference Documentation for Consumers and Engineers

In this blog, we examine the differences in documentation needs between consumer products and engineering products.

Enable Application Design without Considering Device Configuration with Distributed Processing Software for Multiple Devices

Enable Application Design without Considering Device Configuration with Distributed Processing Software for Multiple Devices

Renesas is working on the development of a solution that allows developers to develop applications without considering device configuration.

Virtual Platform Co-Simulation for Shift-Left in Vehicle Software Development

Virtual Platform Co-Simulation for Shift-Left in Vehicle Software Development

Renesas' co-simulation environment for multi-devices enables software development with inter-device communication without actual devices for early development of E/E architectures.

RX Blog: RX23E-A Use of common part

Examples of Design Standardization in Sensing Equipment Using the RX23E-A MCU with Built-In High-Precision Delta-Sigma ADC - Blog 1

This blog series introduces standardizing the design of sensing equipment using the RX23E-A MCU’s built-in high-precision delta-sigma ADC. Blog 1 highlights the standardization between models of a product.

Overview of Renesas Automotive Business Strategy

Overview of Renesas Automotive Business Strategy

This blog explains how Renesas views the evolution of the automotive industry and builds its business strategy.

Creating autonomous I/O systems without the need for CPU intervention

Creating autonomous I/O systems without the need for CPU intervention

How we can use the Data Operating Circuit and the Data Transfer Controller to create complete, autonomous subsystems that can make simple decisions based on measured data without CPU intervention.

Renesas Continues Leadership in Data Center with New Chipsets for High Performance Memory Modules Based on DDR5 Multiplexer Combined Ranks (MCR) Dual In-line Memory Module Blog

Renesas Continues Leadership in Data Center with New Chipsets for High Performance Memory Modules Based on DDR5 Multiplexer Combined Ranks (MCR) Dual In-line Memory Module

Multiplexed Register Clock Driver (MRCD) and Multiplexed Data Buffer (MDB) components allow DDR5 memory modules to deliver significantly higher bandwidth for memory sub-systems in next-generation servers.

「ポーター賞」CEO柴田が一橋ビジネススクール楠木教授と対談

「ポーター賞」CEO柴田が一橋ビジネススクール楠木教授と対談

ルネサスは、一橋ビジネススクールが主催する2022年度「ポーター賞」を受賞しました。

Solar Powered Location Tracker

I Can’t Find My Asset! Maybe One Size Asset Tracker Does Not Fit All

Renesas offers a solution that adapts well in remote locations where there is no Wi-Fi or Bluetooth LE access, only a cellular radio using CAT-M1; the inclusion of solar energy harvesting into the design allows for long-term battery life.