Recommending the H8S Family Microcontroller IP to Users Looking For H8/3048-like IP
We strongly recommend using the H8S IP if you are looking for IP for an H8/300H microcontroller such as one from the H8/3048F or H8/3052F group.
We strongly recommend using the H8S IP if you are looking for IP for an H8/300H microcontroller such as one from the H8/3048F or H8/3052F group.
Artificial intelligence (AI) at the edge of the network is a cornerstone that will influence the future direction of technology. If AI is an engine of change, semiconductors are the oil driving the new age.
Renesas Ready Partner Network solutions deliver plug-and-play options to help simplify the design process and accelerate both time to market and time to revenue across the extensive Renesas MPU and MCU platforms.
For model-based development, I would like to introduce Embedded Target for RH850 Virtual Platform, which facilitates early verification and shortening of development period.
We are introducing an Application Note and sample programs as reference for implementing QSPI serial Flash XIP functionality on the RX671.
Instead of custom boards that are difficult to develop, Tomoyuki introduces the RZ-based SoMs and SBCs enabling high-performance HMI development with minimal costs and resources, in a shorter time.
This blog provides an overview of LoRa® and LoRaWAN® communications suitable for IoT and the LoRa-based solutions with low power and easy to design/evaluate features that are available from Renesas.
Introduces the concept of the Data Operating Circuit (DOC) and how it can be used to control smart peripherals without CPU intervention, so improving system determinism and reducing power consumption.
We introduce the RA6T2 evaluation environment that enables immediate evaluation of motors with inductive position sensor IC (IPS2200), and the advantages of inductive position sensor ICs.
Increased automation in the industrial sector can cause unexpected risks. System designers need to implement safety measures. Renesas helps robust solutions but reduces cost and time to market.