Skip to main content

GR-COTTON Special Project: Humidity Temperature Sensor

Overview

This program introduces how to measure temperature and humidity by connecting a humidity/temperature sensor (SHT31) to the GR-COTTON board.

cotton-sp-hdc1000-serial

Preparation

You will need a GR-COTTON board, a USB cable (Micro B type), and an SHT31 humidity/temperature sensor.

You will need to install a pin socket on the GR-COTTON board and a pin header in the SHT31 sensor.

The SHT31 sensor and the pin socket can be purchased from the Akizuki Denshi website.

cotton-sp-prepare-hdc1000

Connect the SHT31 sensor module to GR-COTTON as shown in the photo to the right.

Make sure the white jumper on the reverse side of GR-COTTON is moved to the “3V3 USB” side. If it is set to the BATT side, remove and reinsert it into the USB side.

cotton-sp-prepare-hdc10002
cotton-sp-prepare2

Displaying Temperature and Humidity on the Serial Monitor

The sample below programs the serial monitor to display temperature and humidity values read every second by the humidity/temperature sensor.


#include <arduino.h>
#include <Wire.h>
 
#define SHT31_ADDRESS 0x40
#define SHT31_RDY_PIN 2
  
#define SHT31_TEMPERATURE_POINTER     0x00
#define SHT31_HUMIDITY_POINTER        0x01
#define SHT31_CONFIGURATION_POINTER   0x02
#define SHT31_SERIAL_ID1_POINTER      0xfb
#define SHT31_SERIAL_ID2_POINTER      0xfc
#define SHT31_SERIAL_ID3_POINTER      0xfd
#define SHT31_MANUFACTURER_ID_POINTER 0xfe
 
#define SHT31_CONFIGURE_MSB 0x10 /* Get both temperature and humidity */
#define SHT31_CONFIGURE_LSB 0x00 /* 14 bit resolution */
 
void getTemperatureAndHumidity(float *temperature, float *humidity) {
  unsigned int tData, hData;
  
  Wire.beginTransmission(SHT31_ADDRESS);
  Wire.write(SHT31_TEMPERATURE_POINTER);
  Wire.endTransmission();
  while (digitalRead(SHT31_RDY_PIN) == HIGH);
  Wire.requestFrom(SHT31_ADDRESS, 4);
  while (Wire.available()  < 4);
  
  tData = Wire.read()  << 8;
  tData |= Wire.read();
  
  hData = Wire.read()  << 8;
  hData |= Wire.read();
  
  *temperature = tData / 65536.0 * 165.0 - 40.0;
  *humidity = hData / 65536.0 * 100.0;
}
 
//*********************************************************
void setup() 
{
  setPowerManagementMode(PM_STOP_MODE); // use stop delay
 
  //Initialize Serial and I2C communications
  Serial.begin(9600);
  Wire.begin();
  pinMode(SHT31_RDY_PIN, INPUT);
   
  //Put the SHT31 IC into the correct operating mode
  Wire.beginTransmission(SHT31_ADDRESS);
  Wire.write(SHT31_CONFIGURATION_POINTER);
  Wire.write(SHT31_CONFIGURE_MSB);
  Wire.write(SHT31_CONFIGURE_LSB);
  Wire.endTransmission();
 
}
//------------------------------------------------------
void loop() 
{
  float temperature, humidity;
  
  getTemperatureAndHumidity(&temperature, &humidity);
  Serial.print("Temperature = ");
  Serial.print(temperature);
  Serial.print(" degree, Humidity = ");
  Serial.print(humidity);
  Serial.println("%");
  Serial.flush();
  
  delay(1000);
 
}


Temperature and Humidity Display for Picalico Reader

Each tap on the touch sensor yields a visible light transmission of temperature and humidity.

Picalico Reader is a smartphone app capable of reading these visible light signals.


#include <arduino.h>
#include <Wire.h>
#include <PicalicoClass.h>
 
Picalico pica(LOW); // set LED to active high
 
#define SHT31_ADDRESS 0x40
#define SHT31_RDY_PIN 2
 
#define SHT31_TEMPERATURE_POINTER     0x00
#define SHT31_HUMIDITY_POINTER        0x01
#define SHT31_CONFIGURATION_POINTER   0x02
#define SHT31_SERIAL_ID1_POINTER      0xfb
#define SHT31_SERIAL_ID2_POINTER      0xfc
#define SHT31_SERIAL_ID3_POINTER      0xfd
#define SHT31_MANUFACTURER_ID_POINTER 0xfe
  
#define SHT31_CONFIGURE_MSB 0x10 /* Get both temperature and humidity */
#define SHT31_CONFIGURE_LSB 0x00 /* 14 bit resolution */
 
void getTemperatureAndHumidity(float *temperature, float *humidity) {
  unsigned int tData, hData;
   
  Wire.beginTransmission(SHT31_ADDRESS);
  Wire.write(SHT31_TEMPERATURE_POINTER);
  Wire.endTransmission();
  while (digitalRead(SHT31_RDY_PIN) == HIGH);
  Wire.requestFrom(SHT31_ADDRESS, 4);
  while (Wire.available() < 4);
   
  tData = Wire.read() << 8;
  tData |= Wire.read();
   
  hData = Wire.read() << 8;
  hData |= Wire.read();
   
  *temperature = tData / 65536.0 * 165.0 - 40.0;
  *humidity = hData / 65536.0 * 100.0;
}
 
//*********************************************************
void setup() 
{ 
  setPowerManagementMode(PM_SNOOZE_MODE, 0, 800); // use snooze
  //Initialize Serial and I2C communications
  Wire.begin();
 
  //Put the SHT31 IC into the correct operating mode
  Wire.beginTransmission(SHT31_ADDRESS);
  Wire.write(SHT31_CONFIGURATION_POINTER);
  Wire.write(SHT31_CONFIGURE_MSB);
  Wire.write(SHT31_CONFIGURE_LSB);
  Wire.endTransmission();
  
}
//------------------------------------------------------
void loop() 
{
  float temperature, humidity;
  static bool g_mode = 0;
   
  analogRead(A6); // into snooze mode, wait for touch.
  pica.attach(22, 23, 24);
  getTemperatureAndHumidity(&temperature, &humidity);
  if(g_mode == 0){
    pica.writeTemperature((int)temperature); // write temperature into picalico
  } else {
    pica.writePercent((int)humidity); // write temperature into picalico
  }
  delay(10000); // operate 10sec
  g_mode = !g_mode;
  pica.detach();
    
}

cotton-sp-picalico