Skip to main content

GR-COTTON Special Project: Having Fun with LEDs

Overview

Here we introduce several ways to enjoy GR-COTTON LED lighting.

Simply copy and paste the sample programs to the Web compiler and IDE for GR.

cotton-sp-congratulation

Preparation

You will need a GR-COTTON board and a USB cable (Micro B type).

Make sure the white jumper on the reverse side of GR-COTTON is moved to the “3V3 USB” side. If it is set to the BATT side, remove and reinsert it into the USB side.

cotton-sp-prepare
cotton-sp-prepare2

The following sample is extremely easy to follow, and only makes the blue LED blink.

The blue LED is allocated to pin 24 on the GR-COTTON board. It is output from pin 24 in pinMode, and turned ON and OFF with digitalWrite.

Pin 22 is red and pin 23 is green, so set the #define area to 22 or 23 to change LED colors.


#include <arduino.h>

#define LED 24 // blue led
void setup() {
    pinMode(LED, OUTPUT);
    digitalWrite(LED, HIGH);
}



void loop() {
    digitalWrite(LED, LOW);
    delay(500);
    digitalWrite(LED, HIGH);
    delay(500);
}

Programming the LED to Flicker Like a Firefly

The sample shows how to make the red and green LEDs flicker like a firefly. The intensity of the LED light can be set by configuring area 0 - 255 using analogWrite; digitalWrite was used only to turn the LEDs ON and OFF.


#include <arduino.h>

#define LED_R 22 // red led
#define LED_G 23 // green led
void setup() {
}

void loop() {
    for(int i = 0; i < 255; i++){
    analogWrite(LED_R, i);
    analogWrite(LED_G, i);
    delay(5);
    }
    for(int i = 0; i < 255; i++){
    analogWrite(LED_R, 255 - i);
    analogWrite(LED_G, 255 - i);
    delay(5);
    }
}

Rainbow

The sample below shows how to make the LEDs flicker in a rainbow of colors.


#include <arduino.h>

void setup() {
}

void loop() {
    static double t = 0.0;
    analogWrite(22, int(255.0 * pow(0.5 - 0.49 * cos(t / 2.0), 2.0)));
    analogWrite(23, int(255.0 * pow(0.5 - 0.49 * cos(t / 3.0), 2.0)));
    analogWrite(24, int(255.0 * pow(0.5 - 0.49 * cos(t / 5.0), 2.0)));
    t = fmod(t + (2 * M_PI / 1000 * 10), 60.0 * M_PI);
    delay(1);
}