Basic Library
Digital I/O
Analog I/O
Advanced I/O
Time
Math
Trigonometry
Random Numbers
Bits and Bytes
Interrupts
Serial Comm.
Standard Library
Ethernet
Ethernet (Server)
Ethernet (Client)
Servo Motor
Character LCD
SPI
I2C (Wire)
SD Card
SD (File Operations)
Periodic Operation
Clock (RTC)
Digital I/O
This library is for configuring the digital signal (HIGH/LOW) to function as either input or output.
pinMode
- Description
- Configures the specified pin to behave either as an input or an output.
- Syntax
- pinMode(pin, mode)
- Parameters
- pin: The number of the pin to set
mode: INPUT or OUTPUT - Returns
- None
digitalWrite
- Description
- Write a HIGH or a LOW value to a digital pin.
- Syntax
- digitalWrite(uint8_t pin, uint8_t value)
- Parameters
- pin: The pin number
value: HIGH or LOW - Returns
- None
digitalRead
- Description
- Reads the value from a specified digital pin, either HIGH or LOW.
- Syntax
- digitalRead(uint8_t pin)
- Parameters
- pin: The pin number
- Returns
- HIGH or LOW
Sample Program
Sample for digitalWrite and digitalRead.
#include <Arduino.h>
#define INTERVAL 100
void setup()
{
pinMode(PIN_LED_RED , OUTPUT);
pinMode(PIN_LED_GREEN , OUTPUT);
pinMode(PIN_LED_BLUE , OUTPUT);
pinMode(PIN_LED_USER , OUTPUT);
pinMode(PIN_SW , INPUT);
}
void loop()
{
while(digitalRead(PIN_SW) == 0){
digitalWrite(PIN_LED_USER, 1);
delay(INTERVAL);
digitalWrite(PIN_LED_USER, 0);
delay(INTERVAL);
}
digitalWrite(PIN_LED_RED, 1);
delay(INTERVAL);
digitalWrite(PIN_LED_RED, 0);
digitalWrite(PIN_LED_GREEN, 1);
delay(INTERVAL);
digitalWrite(PIN_LED_GREEN, 0);
digitalWrite(PIN_LED_BLUE, 1);
delay(INTERVAL);
digitalWrite(PIN_LED_BLUE, 0);
}
Support
Support Communities
Get quick technical support online from Renesas Engineering Community technical staff.
Knowledge Base
Browse our knowledge base for helpful articles, FAQs, and other useful resources.