Basic Library
Digital I/O
Analog I/O
Advanced I/O
Time
Math
Trigonometry
Random Numbers
Bits and Bytes
Interrupts
Serial Comm.
Standard Library
Ethernet
Ethernet (Server)
Ethernet (Client)
Servo Motor
Character LCD
SPI
I2C (Wire)
SD Card
SD (File Operations)
Periodic Operation
Clock (RTC)
Math
This library performs all types of calculations including min/max, absolute value and the square root of a number. Users can also constrain a number within a range, re-map a number from one range to another, and calculate the value of a number raised to a power.
min
- Description
- Compares two values, returns the smaller one.
- Syntax
- min(x, y)
- Parameters
- x: The first number, any data type
y: The second number, any data type - Returns
- The smaller of the two parameter values.
max
- Description
- Compares two values, returns the larger one.
- Syntax
- max(x, y)
- Parameters
- x: The first number, any data type
y: The second number, any data type - Returns
- The larger of the two parameter values.
abs
- Description
- Computes and returns the absolute value of a number.
- Syntax
- abs(x)
- Parameters
- x: The number to be converted
- Returns
- If x is greater than or equal to 0, returns x; if less than 0, returns -x.
constrain
- Description
- Constrains a number to be within a range.
- Syntax
- constrain(x, a, b)
- Parameters
- x: The number to constrain, all data types
a: The lower end of the range, all data types
b: The upper end of the range, all data types - Returns
- If x is between a and b, returns x; if x is less than a, returns a; if x is greater than b, returns b.
amap
- Description
- Re-maps a number from one range to another. For example, when the value is 5 within the range of 0 to 10, it is re-mapped to 50 in the range of 0 to 100.
- Syntax
- amap(value, fromLow, fromHigh, toLow, toHigh)
- Parameters
- value: The number to map
fromLow: The lower bound of the value's current range
fromHigh: The upper bound of the value's current range
toLow: The lower bound of the value's target range
toHigh: The upper bound of the value's target range - Returns
- The value after mapping
pow
- Description
- Calculates power (exponential).
- Syntax
- pow(base, exponent)
- Parameters
- base: Any value; (float)
exponent: The power to which the base is raised (float) - Returns
- The result of the exponentiation (double)
sqrt
- Description
- Calculates the square root of a number.
- Syntax
- sqrt(x)
- Parameters
- x: The number, any value
- Returns
- Double, the number's square root.
Sample Program
Sample using constrain and pow.
#include <Arduino.h>
void setup(){
Serial.begin(9600);
}
void loop(){
Serial.println("Calculate the area of a circle ");
Serial.println("Input value 0-9");
while(!Serial.available());
int d = Serial.read();
d = constrain(d - 0x30, 0, 9); //convert from ASCII to numeric, and remove error value
Serial.print(d);
Serial.print(" x ");
Serial.print(d);
Serial.print(" x 3.14 = ");
Serial.println(pow(d, 2) * PI);
}