Skip to main content
Renesas Electronics Corporation

Overview

Description

GR-PEACH is the Gadget Renesas board for the Renesas RZ family's RZ/A1H group of microprocessor (MPU) products. Fully pin-compatible with the Arduino UNO, GR-PEACH is an Arm® Mbed™-enabled development platform. GR-PEACH takes advantage of web browser-based program development and a robust library selection. With the added appeal of 10MB of built-in RAM and the processing power of Arm Cortex™-A, GR-PEACH was created for the developer interested in high-speed prototyping of IoT devices with loads of HMI—graphics, touch panel, camera input, audio, network and more.

In addition, GR-PEACH supports multiple platforms, .NET Micro Framework (MF), Arduino, and TOPPERS/ASP (RTOS).

Get Started

Technical Information

Board Distributors

GR-PEACH boards and other shields can be purchased through the following sites:

Features

  • Embeds Arm Cortex-A RZ/A1H (R7S721001VCBG) and Arduino UNO pin compatibility supports various shields.
  • GR-PEACH board is equipped with a LAN connector (RJ-45) and connectors for Arduino UNO-compatible pins and service pins
  • Enables camera and Wi-Fi connection with the GR-PEACH board. Camera specifications are VGA 640 x 480, maximum 60fps, and a horizontal angle view of 98 degrees
  • Enables stereo plug, camera module, and USB host connection with GR-PEACH. Note: A camera module is not included. MT9V111 is recommended
  • 4.3-inch wide display with touch panel. Note: GR-PEACH-FULL cannot be used for this shield. Refer to the Corestaff vendor's site for the use details

Applications

Documentation

Design & Development

Software & Tools

Software Downloads

Sample Code

Resources

Schematic/Design

Sketch Reference

  • GR-PEACH Sketch Reference

How to Program


Project File for e2 studio

Project file for sketching in Eclipse-based development environment e2 studio. For downloading and installing e2 studio, please refer to the e2 studio product page.

You can import as an archive file (zip) as an existing workspace from the e2 studio menu "File" -> "Import".

Do the menu "Project" -> "Update all dependencies" at the initial build. Only sources changed since the next build will be compiled.

DisplayApp

DisplayApp is an application that displays the camera image sent by USB CDC.

Installing the USB driver is required on versions earlier than Windows 10.

Below is an Arduino-like sketch example.

    
            #include <Arduino.h>
            #include <Camera.h>
            #include "DisplayApp.h"
            Camera camera;
            static DisplayApp display_app;
            void setup() {
                camera.begin();
            }
             
            void loop() {
                display_app.SendJpeg(camera.getJpegAdr(), (int)camera.createJpeg());
                delay(10);
            }
            }
            

Support

Support Communities

  1. GR-PEACH Board debugging with NXP DAPLink CMSIS-DAP Usb Interface

    Hello, I need to debug an application on GR-PEACH board using the USB interface using the OpenOCD Debugger. I have configured the the debugger in my project in this way: But when I start the debugging the console shows the message below but the debugger doesn't break at ...

    Feb 20, 2023
  2. Where is executed the code on RZ/A1H-Starter-Kit-Plus and GR-PEACH.

    Hello, I'm trying the code present in the examples r01an5093ej0110-rza1-swpkg for rsk demoboard and r01an5397ej0110-rza1-swpkg-grpeach for GR_PEACH. Loading the executable with J-Link Lite I see that all the addresses of the code refer to addresses of the subsequent to 0x18080000, which if ...

    Mar 1, 2023
  3. RZ/A1 ETHER samples

    Hi, I have not found any samples for the Ethernet controller of RZ/A1H or RZ/A1L in Application Notes and Sample Code http://www.renesas.eu/products/mpumcu/rz/rza/Application_Notes.jsp Are there any samples for the ETHER ...

    Nov 17, 2015
View All Results from Support Communities (7)