Skip to main content

Interrupts

Interrupts

This library allows users to trigger a process interrupt function or enable/disable an interrupt function when the input to a pin changes value.

attachInterrupt

Description
Specifies a function to execute (call) when an external interrupt occurs (signal on external pin).
Syntax
attachInterrupt(pin, void(*)(void) func, mode)
Parameters
pin: The number of the interrupt number. Specify X of IntX described in the PinMap.
func: The function to call when the interrupt occurs
mode:
LOW (to trigger the interrupt whenever the pin is low)
CHANGE (to trigger the interrupt whenever the pin changes value)
FALLING (to trigger when the pin goes from high to low)
RISING (to trigger when the pin goes from low to high)
Returns
None

detachInterrupt

Description
Turns off the interrupt specified in attachInterrupt.
Syntax
detatachInterrupt(pin)
Parameters
pin: The number of the interrupt number.
Returns
None

interrupts

Description
Re-enables the interrupt disabled in noInterrupts.
Syntax
interrupts()
Parameters
None
Returns
None

noInterrupts

Description
Disables an interrupt process. Use this when you need to protect the timing of a specific process; this can even be used to disable an important task run in the background.
Syntax
noInterrupts()
Parameters
None
Returns
None

Sample Program

This is a sample that generates an interrupt when you press SW0 (Int4).


#include <Arduino.h>

int ledpin = PIN_LED_BLUE;
int intpin = 1;
volatile int state = LOW;
void blink()
{
  state = !state;
}
  
void setup()
{
  pinMode(ledpin, OUTPUT);
  pinMode(intpin, INPUT_PULLUP);
 
  attachInterrupt(0, blink, CHANGE);
}
  
void loop()
{
  digitalWrite(ledpin, state);
}