Skip to main content

Overview

Description

e² studio is an Eclipse-based integrated development environment (IDE) for Renesas MCUs. In addition to Eclipse’s own powerful code editor, e² studio offers a rich range of extended functions. e² studio covers all development processes, from the downloading of sample code to debugging.

We provide the platform installer includes Flexible Software Package (FSP) and e² studio for users using FSP support RZ Family products. For more detail, see Release Information.

Release Information

ArchitectureVer.Released
64-bit version2025-12Dec 12, 2025
32-bit version (Note)V7.8.0Apr 20, 2020

Note

Henceforth, only the 64-bit version of the e² studio is to have regular updates. Updates to the 32-bit version of the e² studio, on the other hand, will be limited to essential modifications.

FSP Platform installer for RZ Family

It can be obtained as a platform installer from the FSP page for each RZ family series. Click a ‘Flexible Software Package (FSP) Platform Installer of e² studio (and Smart Configurator)’ on ‘Downloads’ list.

Information on Usage

Installation, Building and Debugging: e² studio Integrated Development Environment User's Manual: Getting Started RENESAS MCU RZ Family (PDF | English, 日本語)

Generating Code

Device groupsRelated documents, Related product pages
RZ/A2MRZ/A2M Smart Configurator User Guide: e² studio (PDF | English, 日本語)
Details of the RZ/A2M Software Package
RZ/A3ULRZ/A Getting Started with Flexible Software Package V3.61 (Deprecated) (PDF)
Details of the RZ/A3UL Software Package
RZ/T2M, RZ/T2ME, RZ/T2L, RZ/N2L, RZ/T2H, RZ/N2HRZ/T2, RZ/N2 Getting Started with Flexible Software Package V3.10 (Deprecated) (PDF)
RZ/G2L, RZ/G2LC, RZ/G2UL, RZ/G3SRZ/G Multi-OS Package
RZ/V2H, RZ/V2N, RZ/V2LRZ/V Multi-OS Package

 

FAQ

Title
e² studio FAQs
Where can I find e² studio tutorial?
Project Migration from CS+ to e² studio

See all related FAQs

Target Devices

Note

We provide the platform installer includes Flexible Software Package (FSP) and e² studio for users using FSP support RZ Family products. For more detail, see Release Information.

Downloads

Documentation

Design & Development

Videos & Training

Additional Details

e² studio

See the table below for features of the software and tools available for use with the e² studio on RZ-family products.
For an overview of the functions and features of the e² studio, refer to e² studio (the general page).

Support for code generation and other useful functions for the RZ family

Tool nameDescription
Smart ConfiguratorA GUI-based tool that provides support for downloading and importing middleware for code generation and configuring various settings
Smart ManualA function that allows you to find various information in a hardware manual, such as on registers, without opening the actual hardware manual
Smart BrowserA function that allows you to easily search and show the latest version of the hardware manual, technical updates, application notes, and tool news for the Renesas microcontroller you are using

 

Compilers for the RZ Family

Supported CompilerInformation on Usage
Open Source
GNU Arm Embedded
  • The GNU compilers can be installed through selection with the installer of the e² studio. This requires an Internet connection.
    Also, the GNU tools for each family can be installed free of charge by downloading them from the GNU Web site (registration is required for the e² studio which has already been installed).
    GCC6.2; 6-2016-q4-major and later versions: arm Developer
    GCC 5.4; 5-2016-q3-updated version: Launchpad.ne
    Relation between GCC version and toolchain version

 

Debugging tools for the RZ Family

  • Segger J-Link (Note1)

Note

  1. Product from a Renesas partner

 

QE: Tools for Particular Applications for the RZ Family

Details: QE(Quick and Effective tool solution)

 

Simpler Development of IoT Devices Connectable with Cloud Service

The e² studio supports the development of software for IoT devices to be connectable with Amazon Web Services (AWS) or Microsoft Azure Cloud Computing Service. The e² studio offers the following powerful functions for FreeRTOS or Azure RTOS.

  • Quick building after downloading the latest version of FreeRTOS or Azure RTOS project directly from GitHub®
  • Assisting in configuring RTOS, all required drivers, network stacks (TCP/IP, Wi-Fi, and MQTT), and component libraries (Device Shadow, Azure RTOS NetX duo so on)(Note1)
  • Embedding additional middleware and drivers (such as for USB and file-system support) in IoT devices
Image
The e² studio supports the development of software for IoT devices to be connectable with Amazon Web Services (AWS)

Note

  1. The settable components of RTOS are as follows: MQTT, Greengrass Discovery, Device Shadow, Azure RTOS NetX duo , Secure Sockets, and TCP/IP

Support

Support Communities

  1. e2studio "Managed Build system manifest file error"

    ... t contain this option anyway, so i have no idea what this message means and how can i repair it. I'm using the following e2studio: Version: 2024-10 (24.10.0) Build Id: R20241003-1714 The projects are for RZ/N2H, if it does matter. Is it possible ...

    Aug 11, 2025
  2. Renesas synergy MCU on VSCode

    ... use for my project an Renesas Synergy S5D97 and i want to know if is it possible to use vscode for building and debugging this Renesas. I found user's guide but only for RA, RCAR, RE, RL78, RX or RZ family. Is there a way for Synergy family ? Thanks

    Feb 20, 2024
  3. openocd support for RA4M2

    Hi, Is there openocd support for RA4M2? According openocd source code, we find out support only for r7s72100, rcar_gen[2,3], rcar_reset_common, rz_g2 and s7g2. What we need to flash the device using openocd tool.

    Feb 3, 2022
View All Results from Support Communities (5)

Knowledge Base

  1. Where Can I Find the e² studio Tutorials?

    ... at the e2 studio information web page for each device family. The manual shows basics of operation. It is recommended to read it through.e2 studio for RA Family: https://www.renesas.com/e2studio-rae2 studio for RZ Family: https://www.renesas.com/e2studio ...

    Dec 28, 2022
  2. Differences between e² studio and CS+ Integrated Development Environments

    ... studio, CS+. For more information, see the IDE Release Notes and the respective documentation. [Supported Device Families]e² studioCS+ (CS+ for CC) CS+ (CS+ for CA,CX) RX, RL78, RH850,RA, RZ, RE,Renesas Synergy™,RISC-V MCU RX, RL78, RH850 RL78, 78K, V850 [Supported Compilers]e² studio ...

    Oct 9, 2024
  3. Command-line build of e² studio project

    ... not be due to the build failure.For projects that use FSP (RA family and some RZ family), generate and build a project with the e² studio GUI version, and then try building on the command line. More information is available in e² studio Help at "Using e² studio in ...

    Mar 25, 2024
View All Results from Knowledge Base (5)
Support Communities

Support Communities

Get quick technical support online from Renesas Engineering Community technical staff.
Browse Articles

Knowledge Base

Browse our knowledge base for helpful articles, FAQs, and other useful resources.
Submit a Ticket

Submit a Ticket

Need to ask a technical question or share confidential information?