Ultra-Low-Power Wi-Fi + Bluetooth Low Energy Combo Pmod Board
The US159-DA16600EVZ is a highly integrated ultra-low-power Wi-Fi + Bluetooth® Low Energy (LE) combo Pmod™ module that provides a convenient way to add both low-power...
Heat pumps offer the most energy-efficient and green way to provide heating and cooling in many applications, as they extract heat from a source (air, water, ground) to increase the temperature of water/air for domestic heating or sanitary hot water. Thanks to the energy transfer by the Carnot process (i.e. reversed fridge), heat pumps have an electric energy efficiency of up to 400%.
This solution provides a cost-effective and low-power smart controller for any heat pump, such as a smart heat pump. Thanks to our feature-rich MCU and a wide spectrum of wireless communication solutions the user can change the thermostat, set temperature schedules, and review the energy consumption and air quality.
System Benefits:
Select a block to discover products for your design
Skip interactive block diagramThe US159-DA16600EVZ is a highly integrated ultra-low-power Wi-Fi + Bluetooth® Low Energy (LE) combo Pmod™ module that provides a convenient way to add both low-power...
![]() |
Smart Heat Pump |
![]() |
Arduino Nicla Smart Sensor Module |