Skip to main content

Master Actuator for Automatic Home or Building HVAC System

Overview

Description

The master actuator unit(s) is the brain of the HVAC system. It fulfills all of the functions of a slave actuator unit and includes other capabilities, such as: ​

  • Collection of all sensors data from indoor sensor unit(s), outdoor sensor unit(s) and slave actuator unit(s)​
  • Additional weather information may be collected from the internet, if an IP gateway is implemented in the master actuator or separately (see IP Gateway for Automatic Home or Building HVAC System) ​
  • Calculation/Determination of the set points for each slave actuator unit, like flow direction (in/out), temperature, etc., using an algorithm or the latest embedded artificial intelligence (AI) technology​
  • Provision of the set points for each slave actuator and the master itself​
  • Local (graphical) GUI of the whole system, which may also be mirrored by a Bluetooth® or web interface​
  • Real-time clock (RTC) and its distribution to sensor/actuator units for different operation modes, depending on the day, time, holiday, etc.​

​From a system perspective, the master and slave actuator can have the same hardware and software. In this case, the master is a role rather than a certain device and it would not represent a single-point-of-failure, as another slave actuator could take over the master role in case the original master fails. However, there must be only one master, per system, at a time.​

System Benefits​:

  • The RX23W MCU enables Bluetooth 5 mesh communication​
  • The master actuator can (but does not need to) have an integrated gateway to the intranet/internet using a secure communication mechanism like HTTPS or MQTT, if not achieved externally (see IP Gateway for Automatic Home or Building HVAC System). For these cases, one or multiple of the following technologies are available:​
    • Wi-Fi (based on IEEE 802.11), Thread or Zigbee (based on IEEE 802.15.4), Ethernet (based on IEEE 802.3), LTE-M/-NB (depending on geographical region and available providers), or LoRaWAN​

*Note: For the power supply, usually the mains will be needed for the fan/HVAC (e.g., 230Vac or 110Vac, or 24Vdc from the building control system).

Comparison

Applications

Winning Combinations Interactive Diagram

Select a block to discover products for your design

Template 1 Master Fan Control Board Master Fan Control Board Master Fan Control Board Sheet.430 Antenna Sheet.423 Sheet.424 Sheet.425 Sheet.426 Sheet.427 Connector Line.429 Connector Line.411 Horizontal Wire Bundle Communication Lines B.795 2 2 2 Connector Line.406 Connector Line.390 Connector Line.391 Connector Line.392 Connector Line.385 Connector Line.382 Connector dotted line.366 Connector dotted line.367 Connector dotted line.369 Connector dotted line.370 Connector dotted line.371 Ext. Supply e.g. 24V Ext. Supply e.g. 24V Ext. Supply e.g. 24V EU079 EU079 EU079 Connector Line Connector Line.326 Connector Line.327 Vertical Wire Bundle Label Text 10pt.1046 2 2 Sheet.331 Vertical Wire Bundle.332 Label Text 10pt.1046 2 2 Sheet.334 Vertical Wire Bundle.335 Label Text 10pt.1046 2 2 Sheet.337 Connector Line.339 Connector Line.340 Motor Sheet.342 Sheet.343 M M Connector Line.344 LV BLDC Motor LV BLDC Motor LV BLDC Motor Vertical Wire Bundle.346 6 6 6 Sheet.348 Vertical Wire Bundle.349 3 3 3 Sheet.351 Connector Line.352 Connector Arrow Connector dotted arrow LV DC Supply LV DC Supply LV DC Supply Connector dotted line Connector Line.386 Connector Line.387 Connector 1.160 Connector 1.160.389 Vertical Wire Bundle.393 2 2 2 Sheet.395 Vertical Wire Bundle.396 2 2 2 Sheet.398 Vertical Wire Bundle.399 2 2 2 Sheet.401 Connector Line.402 Connector 1.160.403 12V 12V 12V 3V3 3V3 3V3 Connector Line.409 Connector 1.160.410 Buck Regulator Buck Regulator Buck Regulator Buck-Regulator Buck Regulator Buck Regulator Low Pass Filter Low Pass Filter Low Pass Filter Half-Bridge Driver Half-Bridge Driver Half-Bridge Driver Half Bridge Driver Half-Bridge Driver Half-Bridge Driver Half-Bridge Driver Half-Bridge Driver Half-Bridge Driver LCD LCD LCD Cap Touch Sensors Cap Touch Sensors Cap Touch Sensors Cat5/7 PHY Cat5/7 PHY Cat5/7 PHY Wi-Fi, LTE-M/NB-IoT, Lora, etc. Wi-Fi, Lora, LTE-M/NB-IoT, etc. Wi-Fi, Lora,LTE-M/NB-IoT, etc. Flow Sensor Flow Sensor Flow Sensor Hall Sensor Hall Sensor Hall Sensor MOSFET Bank x6 MOSFET Bank x6 MOSFETBank x6 Sheet.415 Microcontroller MCU MCU LCD I/F LCD I/F LCD I/F Cap Touch Cap Touch Cap Touch Ethernet Ethernet Ethernet Serial I/F Serial I/F Serial I/F Flow Sensor I/F or ADC Flow Sensor I/F or ADC Flow Sensor I/F or ADC SCI SCI SCI PWM x6 PWM x6 PWM x6 ADC x3 ADC x3 ADC x3 Label Text 10pt.408 VDD VDD Connector Line.416 Connector 1.160.417 Vertical Wire Bundle.418 3 3 3 Sheet.420 Sheet.433 MCU MCU MCU SCI.379 SCI SCI Label Text 10pt.262 VDD VDD BLE5 PHY BLE5 PHY BLE5 PHY
Exiting Interactive Block Diagram