Skip to main content

RL78/G24 Motor Control Solution: How to Utilize a Solution for Motor Control (2/2)

Feb 26, 2025

This video explains how the motor control solution for the RL78/G24 can be used to easily drive motors using sensorless vector control.

In Part two, we will begin by explaining how to design and adjust the parameters required for sensorless vector control with the RL78/G24. Next, we will outline the procedure for easily evaluating the validity of these parameters using the driving test function. After exporting the parameter information as header files and incorporating them into the sample program, we will introduce examples of motor control evaluation using the analyzer function of Renesas Motor Workbench.

Watch the first part of this video series here.

Chapter's Title

0:00 Parameter design and adjustment on the Etuner function of RMW
1:36 Driving test on the tuner function of RMW
2:45 Reflection of parameters on sample software
3:22 Evaluation of motor control on the analyzer function of RMW

Related Resources