Renesas held a successful European R-Car Consortium (RCC) Forum in March, an annual event that encourages fruitful exchange and networking between Renesas R-Car partners and customers.
With over 250 partners around the world, the RCC is sparking innovation by making available to car OEMs & Tier 1s a large database of system solutions and sharing R-car based demo solutions. 33 of these technology partners went on to participate at the recent European RCC Forum held on March 14 in Duesseldorf, which focused on “Automated & Connected Driving Innovations: From cloud services to sensing, cognitive & control”.
Check out the photo coverage of the event.
2019年3月21日