Results: 68 webinars
RZ/A2Mは、モバイル機器で広く使われているMIPIカメラインタフェースに対応し、HMI(ヒューマン・マシン・インタフェース)の中でもカメラを使ったアプリケーションに適しています。特に、画像処理向けの大きな特長として、入力画像を高速処理する動的再構成プロセッサ (DRP ; Dynamically Reconfigurable Processor)を搭載しています。DRPはRZシリーズの一部製品に内蔵された特殊なハードウェアであり、従来の組込プロセッサに比べ10倍以上高速な画像処理が実現できるアクセラレータとして、家電から産業機器まで幅広いシステムの画像認識アプリケーションに適用できます。本オンラインセミナーでは、世界で最も低価格でDRPに触れられるMbed™対応ボードであるGR-MANGOと、無償提供するFreeRTOS™ベースのソフトウェアパッケージを用いて、同梱するDRP Libraryを活用したリアルタイム画像処理のご紹介と実際の使用方法をレクチャーします。
Years of experience with smartphones has taught us to expect a fluid and intuitive user interface on a touchscreen. As touch user interfaces spread to a wider range of devices, device manufacturers are facing challenges as they struggle to deliver a smartphone-like user experience, especially in lower-cost products and markets. Nothing is more likely to break a user’s trust in a device than a touch interface whose response lags their input by too long, or which cannot react consistently to multiple touches. This webinar takes a look at how Qt on Renesas RA6 MCUs can address these concerns.
In this webinar you will learn about the following:
Basic Audio Front End architecture and concepts for voice user interface
Product design considerations for adding voice
Features and capabilities of the Renesas RA6M5 MCU + DSP Concepts TalkTo Audio Front End solution
Basic Audio Front End architecture and concepts for voice user interface
Product design considerations for adding voice
Features and capabilities of the Renesas RA6M5 MCU + DSP Concepts TalkTo Audio Front End solution
Microcontrollers & Microprocessors
This webinar discusses how Renesas enables endpoint intelligence by providing efficient, flexible, and scalable RZ MPU products for e-AI applications.
In this webinar, participants will learn how Qeexo’s AutoML machine learning platform transforms the embedded Artificial Intelligence (e‑AI) development process without users having to code. Qeexo AutoML is a fully‑automated, end‑to‑end machine learning platform that builds lightweight machine learning solutions (tinyML) running locally on constrained environments such as a Cortex Arm M4 MCU. It augments the user experience and applicability of products like the RA Family of MCUs, adding intelligence with AI for many applications including Wearables, Industrial, Mobile, Smart Home/Appliance and other IoT markets.
The integration of semiconductors into drive technology is opening up entirely new fields of application. In this part we will give insights into the motor control market and we will talk about latest trends. Latest informational Update about the Renesas RA Arm Cortex based on comprehensive and sophisticated Motor Control Line Up. Learn about the flexible and smart functionalities within. Check the easy to use motor control reference solutions provided by Renesas enabling acceleration of your own development, keeping your efficiency by increasing the same and helping you to get faster time to market.
このオンラインセミナーの受講で次のことができるようになります。
周辺機能とセキュリティを実装することでIoT Edgeのパフォーマンスを向上
RL78/G23で低消費電力を実現
強化された周辺機能を使用して、既存のマイコンから容易に移行可能
Easy-to-Useな開発環境を活用して開発を加速(Smart Configurator)
周辺機能とセキュリティを実装することでIoT Edgeのパフォーマンスを向上
RL78/G23で低消費電力を実現
強化された周辺機能を使用して、既存のマイコンから容易に移行可能
Easy-to-Useな開発環境を活用して開発を加速(Smart Configurator)
Microcontrollers & Microprocessors
Modern applications requires more and more user interfacing as well as improved User eXperience (UX). Graphical User Interface (GUI) together with touch screen capability are kind of “new standard” also in embedded applications. Going beyond traditional embedded programming experience many of the engineers still delay a decision of moving forward with embedded Real-Time Operating System (RTOS) as a prerequisite for real-time multitasked operations including GUI, touch interface, sensor readings, communication and various actuation controls.
Our technology is perfect for the design of more traditional touch-like buttons, wheels and sliders, but now designers can also embrace touchless control or material detection applications too! The COVID-19 pandemic has created a strong demand for ‘non-contact HMI' to avoid further contamination, and Renesas has developed multiple solutions to address this need. Renesas Capacitive Touch technology can detect proximity, gestures and materials, for applications such as power switches or door-opening systems, and it's served by solutions that simplify design, lower cost and reduce effects from external noise sources, such as light.
Microcontrollers & Microprocessors
ONE Tech’s MicroAI™ technology brings the capability to locally train machine learning anomaly detection models directly on Renesas RA MCUs. This allows for OEMs to reduce data expenditures, while increasing the level of insight into the performance of their assets without the need for extensive data science.
In this webinar you will learn:
Key design considerations for implementing voice in your constrained IoT applications
How to get started with your design using Renesas RA MCUs and the powerful Cyberon DSpotter toolchain
Key design considerations for implementing voice in your constrained IoT applications
How to get started with your design using Renesas RA MCUs and the powerful Cyberon DSpotter toolchain
この脅威に対抗するためIoTデバイスは自律したセキュリティが必要であり、RX MCUのセキュリティソリューションを活用すればそれを簡単に実現できます。また、IoTデバイスの動作の起点となるMCUを活用したセキュリティの実現は、安全性を強化できます。本セミナーから、以下の情報が取得できます。
セキュリテイ実現に向けた課題
課題を解決するRX MCUのハードウエアセキュリティ機能を起点としたセキュリティソリューション
RX MCUと連携したセキュリティ機能の実現をサポートするパートナーソリューション
セキュリテイ実現に向けた課題
課題を解決するRX MCUのハードウエアセキュリティ機能を起点としたセキュリティソリューション
RX MCUと連携したセキュリティ機能の実現をサポートするパートナーソリューション
Microcontrollers & Microprocessors
Communications Infrastructure
Building on the hardware security foundation in Renesas RA MCUs and RZ MPUs, this webinar will look at how SmartAxiom uses light embedded blockchain technology to deliver such an endpoint-to-cloud solution in a responsive, scalable, and reliable manner. The SmartAxiom solution also eases mass provisioning, reduces operational costs by minimizing the number of keys and certificates, and satisfies the requirements of a Zero Trust environment.
Microcontrollers & Microprocessors
Communications Infrastructure, Consumer Electronics, Industrial, Medical & Healthcare
In this webinar, we will explore the newest member of the RA family. The RA4M2 MCUs offer lowest active power and 100MHz performance simultaneously. This is making the RA4M2 Group ideal for an IoT application platform with a rich variety of different end-products all based on the RA family of microcontrollers.
そこで、本オンデマンドセミナーでは、ユーザビリティ向上の鍵となる静電容量タッチキーや非接触インターフェース、Graphical User Interface (GUI) などの技術を紹介し、これらを導入する上での課題に対して、ルネサスが提供するソリューションをご紹介していきます。