RX23E-A IO-Link Temperature Sensor Solution Development Kit
This single-chip solution uses the 32-bit RX23E-A microcontroller with built-in high-precision analog front-end (AFE) to measure temperature, process sensing and...
This complete industrial sensor network is for temperature controllers, transmitters, data loggers, etc. For IO-Link applications, sensing parameter settings can be done through the IO-Link tool on a PC connected to the user’s IO-Link master board. The device board will be expanded as a universal board, which will be able to connect with various MCU evaluation boards, some RS-485 interfaces, and a controller area network (CAN) with industrial fieldbus. Each connection is independent and the user can select the appropriate connection for their application.
These can be realized by using the RX23E-A or RA2A1 32-bit microcontroller (MCU).
System Benefits:
Available on Lab on the Cloud - Use our PC-based GUI to instantly start configuring and testing.
Launch Lab on the Cloud