DA16200 Ultra-Low Power Wi-Fi Modules Development Kit
The DA16200 development kit is the most ideal way to quickly and easily get started developing applications and products using ultra-low power Wi-Fi.
If you are...
The DA16200 system-on-chip (SoC) is the world's first Wi-Fi SoC to deliver year-plus battery life for always-connected Wi-Fi IoT devices. DA16200 is a low power Wi-Fi networking SoC that delivers a dramatic breakthrough in battery life even for devices that are continuously connected to the Wi-Fi network. In most applications, one year plus battery life is achievable. There is no tradeoff in output power or range, as the SoC's range is industry-leading. The chip also features very strong IoT security, including WPA3 and TLS for authentication and encryption at Wi-Fi and higher stack layers. The DA16200 is a full offload device, meaning the entire Wi-Fi and TCP/IP networking stack and even end product application code can run on-chip with no external CPU or MCU required. Alternatively, a small inexpensive MCU can send the DA16200 commands and the SoC will still perform the full offload networking stack functions.
The DA16200 modules are the perfect complement to the DA16200 ultra-low power Wi-Fi SoC.
Access the industry-leading low power features of the DA16200/DA16600 family simply, quickly and without having to develop any complex software on the Wi-Fi side. To learn more, visit the DA16200 Wi-Fi AT Command Set page.
Software title
|
Software type
|
Company
|
---|---|---|
DA16200 Wi-Fi AT Command Set Simple and fast Wi-Fi implementation using a comprehensive suite of AT-Commands for the DA16200 Wi-Fi and DA16600 Wi-Fi/Bluetooth LE combo products.
|
IDE and Coding Tool | Renesas |
e² studio Eclipse-based Renesas integrated development environment (IDE).
[Support MCU/MPU: RA, RE, RX, RL78, RH850, Renesas Synergy, RZ]
|
IDE and Coding Tool | Renesas |
2 items
|
The DA16200 development kit is the most ideal way to quickly and easily get started developing applications and products using ultra-low power Wi-Fi.
If you are...
Accelerate your IoT development with the DA16200 low power Wi-Fi development kit. The VirtualZero™ based DA16200 development kit makes developing IoT applications easy...
LP WiFi Click is a compact add-on board that represents an ultra-low power Wi-Fi solution. This board features the DA16200, a fully integrated Wi-Fi module with...
SparkFun has teamed up with Arm and Renesas to provide you with this Qwiic WiFi Shield based around the DA16200 module. The DA16200 is a fully integrated Wi-Fi module...
The SparkFun MicroMod DA16200 Function Board adds a fully integrated Wi-Fi module with a 40MHz crystal oscillator, 32.768KHz RTC, Lumped RF filter, 4MB flash memory,...
The SparkFun DA16200 Thing Plus utilizes a highly integrated ultra-low power Wi-Fi system-on-chip (SoC) from Renesas that allows users to develop Wi-Fi and IoT...
The CK-RA6M5 cloud kit enables users to securely connect to the cloud and explore the features of the Cortex®-M33 based RA6M5 group of MCUs and cloud services. With...
The CK-RX65N cloud kit enables users to securely connect to the cloud and explore the features of the Renesas RXv2 core based RX65N MCU Group and cloud services.
With...
The US159-DA16600EVZ is a highly integrated ultra-low-power Wi-Fi + Bluetooth® Low Energy (LE) combo Pmod™ module that provides a convenient way to add both low-power...
This board provides rich connectivity, including Wi-Fi mirroring of mobile screens and Bluetooth® Low Energy (LE) connectivity, and low-cost solutions required for...
The AS043-FGSLEAKPOC2Z Flammable Gas Leakage Detector is a battery-operated, standalone system with wireless connectivity using low-power Wi-Fi communication. This...
The RL78/G23 Indoor Air Quality Sensor Demonstration Board is a demonstration of the unique and powerful features of the RL78/G23. It enables programming and evaluation...
Schematic symbols, PCB footprints, and 3D CAD models from SamacSys can be found by clicking on products in the Product Options table. If a symbol or model isn't available, it can be requested directly from the website.
Matter is single unified IP-based protocol to securely and robustly connect smart devices with each other, regardless of brand, and across smart home ecosystems.
Unlocking Innovation: Renesas Revolutionizes Smart Locks | Blog Post | Apr 15, 2024 |
Renesas Announces Its First Wi-Fi Development Kit with Support for New Matter Protocol | News | Jan 5, 2023 |