メインコンテンツに移動

Dialog Semiconductor Adds Multi-Channel Input Capability to New Nanoamp GreenPAK™ Device

GreenPAKs smallest form factor SLG46811, includes I²C communication interface enabling superior performance and more compact designs

2021年10月1日

London, United Kingdom – Dialog Semiconductor plc (XETRA:DLG), a leading provider of battery and power management, Wi-Fi®, Bluetooth® low energy, and Industrial edge computing solutions, today announced the expansion of their popular GreenPAK™ solution suite with the SLG46811, the market’s smallest GreenPAK device to include an I2C communication interface.

The GreenPAK products are extremely cost effective programmable mixed-signal ASICs that are customer designed with GreenPAK Designer Software. The GreenPAK products feature in many cases sub uA active current consumption, nano second response times, schematic based design and simulation, and tools that allow prototyping and programming when connected to a standard PC USB port. GreenPAK products are widely adopted in the industry with hundreds of millions of units shipped annually to many of the large and trend setting IoT, computing and industrial OEM’s.

The SLG46811 integrates traditional GreenPAK programmable logic with new shift register macrocells, a multichannel sampling analog comparator and a 92 x 8-bit pattern generator, all within a small 1.6mm x 1.6mm package.

The SLG46811 GreenPAK IC eliminates size constraints with the smallest I2C communication interface, with a multichannel sampling comparator capable of sampling four analog signals. Additionally, the shift register macrocells and 92-byte pattern generator allow engineers to take advantage of significant advancements with its nanoamp active current consumption, greater customizability and customer-defined control.

“The SLG46811 is a significant addition to our GreenPAK product family” said John McDonald, Vice President Marketing, CMBU at Dialog Semiconductor. “Current competitive solutions such as discrete logic and analog ICs, Mixed Signal MCUs or small FPGAs are more expensive, have larger footprints, are highly complex, offer higher power consumption and longer latency.

The SLG46811 includes all of these new and traditional features in its ultra-small form factor, achieving a very cost-effective solution improving not only traditional GreenPAK applications but extending GreenPAK products into new functions that allow engineers to create more complex and compact digital projects.”

For more information on the SLG46811, please visit www.dialog-semiconductor.com/products/greenpak/slg46811

For more information on Dialog’s GreenPAK line, please visit: www.dialog-semiconductor.com/products/greenpak


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

この記事をシェアする