メインコンテンツに移動

Dialog Semiconductor Announces SLG47004 GreenPAK™ First Fully Programmable Advanced Analog System IC

Latest GreenPAK™ addition integrates operational amplifiers and digital rheostats, allowing for unique custom analog ICs to be designed practically in minutes, with no associated NRE

2021年10月1日

London, United Kingdom – Dialog Semiconductor plc (XETRA:DLG), a leading provider of battery and power management, Wi-Fi®, Bluetooth® low energy (BLE) and Industrial edge computing solutions, today announced the SLG47004, Dialog’s first Advanced Analog GreenPAK™ IC. The SLG47004 integrates an instrumentation amplifier with auto-trimming, digital pots, analog switches and a myriad of digital functions with in-system programmability in a small 3mm x 3mm solution size allowing designers to create, simulate and prototype their own unique sophisticated analog ICs in minutes at a lower cost than a discrete component implementation.

Similar to the other members of the hugely popular GreenPAK family, the SLG47004 is highly customizable where a vast array of new functions can be simply created by the designer. For example, the SLG47004 includes low offset CMOS operational amplifiers (op amps) with an 8MHz bandwidth, that can be configured into an instrumentation amplifier. The digital potentiometers can be used for auto-trimming the analog system offset or used independently as 10-bit 100kOhm digital rheostats. All this flexible programmability is combined to form a single IC system solution for implementing cost-effective and energy-efficient complete analog system solutions or an Advanced Analog Front End (AFE).

“The SLG47004 is the first GreenPAK IC to now incorporate configurable op amp functionality. Its high level of customization and integration of multiple functions into a single ultra-small form factor device is unmatched by any other solution on the market,” said John Mcdonald, Vice President Marketing, Advanced Mixed Signal Business Group, Dialog Semiconductor. “This new product will rapidly accelerate GreenPAK adoption into entirely new applications for our customers and partners and is just the beginning of a whole new family of solutions extending the GreenPAK family that Dialog will be rolling out,” added Mcdonald.

The SLG47004 is an ideal replacement for designs that include programmable gain amplifiers, instrumentation amplifiers, digital potentiometers, and analog switches. The common applications for the SLG47004 include analog interfaces for sensors, AFEs for Analog-to-digital converters (ADCs), and tunable analog filters. Other potential sensor interface applications include pressure sensors, photo detectors, and force-sensitive button interfaces.

The GreenPAK Designer software package for the SLG47004 allows for fast, accurate and complete analog simulation of the op amps, digital pots, analog switches, comparators, and all digital blocks including some external system components. This allows the designer to simulate circuit nodes both inside and outside the IC. Upon completion of a design, a sample can be easily generated in minutes via the GreenPAK Designer hardware programmer.

The SLG47004 is sampling now and will be in production in the first quarter of 2021. For more information on the SLG47004, please visit: https://www.dialog-semiconductor.com/products/slg47004

For more information on Dialog’s GreenPAK line, please visit: https://www.dialog-semiconductor.com/products/greenpak.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

この記事をシェアする