メインコンテンツに移動

Dialog Semiconductor Connects the Next Generation of Industry 4.0 Devices with Highly Optimized IO-Link IC

Latest IO-Link IC in Dialog’s growing family of Industrial IoT products provides robust connectivity to the smallest, most cost-sensitive IO-Link Devices

2020年2月26日

London, United Kingdom – Dialog Semiconductor plc (XETRA:DLG), a leading provider of power management, charging, AC/DC power conversion, Wi-Fi and Bluetooth® low energy technology, today announced the latest member of its IO-Link product family, the CCE4503. The addition of this new IO-Link IC both expands the company’s reach into the Industrial IoT (IIoT) market and connects the smallest and most price-sensitive IO-Link Device sensors and actuators.

The CCE4503 is the first IO-Link IC to be launched by Dialog following its acquisition of Creative Chips in November 2019 and complements the company’s well-established family of IO-Link Device and Master ICs. IO-Link is the first globally standardized, serial bi-directional point-to-point communication technology (IEC 61131-9) for an industrial automation network. It provides robust communications for the last meters between sensors, actuators and any fieldbus within a network.

The CCE4503 is a highly robust and easy-to-use device-side IO-Link-compliant transceiver that combines IO-Link standard communications with advanced protection circuitry and low power dissipation, within a tiny DFN10 3x3mm package. This makes it possible to add IO-Link connectivity to the most space-constricted industrial sensor and actuator devices. The design has also been rigorously optimized for cost, enabling a greater number of IO-Link devices to benefit from the IO-Link connectivity that provides deeper data access to the cloud.

“Industrial sensors and actuators are integrating more functionality in smaller form factors with greater demands for cloud connectivity,” said Dr. Lutz Porombka, Vice President of Dialog’s Industrial Mixed Signal Business Unit. “The CCE4503 and its optimized feature set is the result of customer-driven demand for a smaller, more cost-efficient IO-Link solution that enables the next generation of Industry 4.0 devices.”

The CCE4503, now currently sampling, is supported by a comprehensive set of development support tools, industry standard IO-Link software and a full-featured customer evaluation board.

For more information about this device, please visit: https://www.dialog-semiconductor.com/products/cce4503

For the latest IO-link video, watch here


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

この記事をシェアする