メインコンテンツに移動

IDT Collaborates with Cavium to Support Hyperscale Data Centers

IDT’s DDR4 Products Deployed in Low-Energy Platform Design for Cavium’s ThunderX® Family of Workload-Optimized ARM Processors 

2016年6月20日

SAN JOSE, Calif., June 20, 2016--Integrated Device Technology, Inc. (IDT) (NASDAQ: IDTI) today announced its collaboration with Cavium, Inc., on a reference design that supports the burgeoning workloads of the hyperscale data center.  The IDT® DDR4 memory interface solutions are incorporated into the reference design, which is built on Cavium’s ThunderX family of workload-optimized 64-bit ARMv8-based processors.

The Cavium ThunderX® reference design can be used to build energy-efficient server solutions featuring IDT’s DDR4 technology. Cavium and its industry partners developed the design to target server solutions for members of the Open Compute Project (OCP) and other hyperscale data center customers.

“IDT’s DDR4 technology offering and the company’s leadership in the OCP High Performance Computing Project made them the obvious choice to team with,” said Rishi Chugh, director, Data Center Processor at Cavium, which similarly has a long history collaborating in the Open Compute community. “Our relationship with IDT enables us to deliver workload-optimized, flexible, scalable and efficient ARM-based server solutions to the data center market, including the growing community of the OCP.”

The ThunderX product family is Cavium’s server processor for next-generation data center and cloud applications, featuring high-performance custom cores, single- and dual-socket configurations, high memory bandwidth and large memory capacity. The product family also includes integrated hardware accelerators, integrated feature-rich high bandwidth network and storage IO, fully virtualized core and IO, and scalable high bandwidth, low latency Ethernet fabric.

IDT’s DDR4 chipset includes register, data buffers and thermal sensors with serial presence detect (SPD). Together, they collectively enable the complete range of unbuffered dual inline memory modules (UDIMMs), registered DIMMs (RDIMMs) and load-reduced DIMMs (LRDIMMs) needed to power the next generation of enterprise and data center servers.

“IDT is excited to work with partners like Cavium and industry bodies like the Open Compute Project to demonstrate the compelling value of our DDR4 chipset in hyperscale data centers,” said Rami Sethi, vice president and general manager of memory interface products at IDT. “Our solution uniquely enables users to scale memory capacity without compromising data rates in order to maximize workload performance and efficiency.”

IDT’s DDR4 memory is part of the company’s vast portfolio of technologies enabling hyperscale data servers, high-performance computing clusters and enterprise servers. IDT also offers digital power management solutions to optimize overall data center performance and power usage, enabling high-density solutions required for space-constrained servers. IDT provides an extensive high-performance timing portfolio, PCIe retimers, PCIe switches and low-latency RapidIO interconnect to enable analytics workloads in the data center.  

The ThunderX reference design is available directly from Cavium.

About IDT

Integrated Device Technology, Inc. develops system-level solutions that optimize its customers' applications. IDT's market-leading products in RF, timing, wireless power transfer, serial switching, interfaces and sensing solutions are among the company's broad array of complete mixed-signal solutions for the communications, computing, consumer, automotive and industrial segments. Headquartered in San Jose, Calif., IDT has design, manufacturing, sales facilities and distribution partners throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol "IDTI." Additional information about IDT is accessible at www.IDT.com. Follow IDT on Facebook, LinkedIn, Twitter, YouTube and Google+.

2016, IDT. IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. ThunderX is a registered trademark of Cavium, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners. 

この記事をシェアする