メインコンテンツに移動

IDT Gas Sensor Gives JAEWONCNC’s In-Car Air Purifier a Sense of Smell

IDT’s ZMOD4410 gas sensor enables JAEWONCNC’s IROAD iair to detect and improve in-cabin air quality.

2019年11月18日

SAN JOSE, Calif., November 18, 2019 – Integrated Device Technology, Inc. (IDT), a wholly owned subsidiary of Renesas Electronics Corporation (TSE: 6723), today announced that its ZMOD4410 gas sensor is at the heart of the IROAD iair in-car air purifier from JAEWONCNC Co. Ltd., a Korean manufacturer of consumer electronics. The ZMOD4410 detects volatile organic chemicals (VOCs) associated with indoor air pollutants, enabling the IROAD iair to inform the consumer about VOC levels.

The IROAD iair is in production and shipping to consumers in South Korea, Japan and India. A USB cable connected to a vehicle’s 12V accessory socket provides the power and its compact size allows for convenient placement anywhere in the vehicle cabin. The device can also be used to monitor and improve the air quality in other environments, such as buildings and the home.

“We created our IROAD iair air purifier to ensure that people can enjoy the substantial health and comfort benefits of clean, odor-free air in their cars – small, tightly enclosed environments where air quality is a major concern,” said Kim Byoung-gyu, chief technology officer at JAEWONCNC. “We selected IDT’s ZMOD4410 gas sensor for its best-in-class sensitivity and its ease of integration, allowing us to get the IROAD iair to market quickly without sacrificing quality or performance.”

“JAEWONCNC’s innovative IROAD iair air purifier is an outstanding example of the growing number of sensor-based products that improve air quality in vehicles, homes, workplaces and other indoor environments,” said Uwe Guenther, general manager of IDT’s industrial group. “Our ZMOD4410 gas sensor is ideal for these and other indoor air quality applications, combining all the characteristics necessary for high volume production without compromising sensitivity or accuracy.”

Complementing its exceptional stability and sensitivity, the ZMOD4410 is also small in size, has low power requirements and features precompiled firmware that allows it to be easily and quickly integrated into product designs.

The ZMOD4410 is based on proven metal oxide (MOx) material and each sensor is electrically and chemically tested to ensure consistency from lot to lot, an important advantage for manufacturers with long production runs. The ZMOD4410 devices are also highly resistant to siloxanes for superior reliability use in harsh applications.

More information about the ZMOD4410 gas sensor is available at www.idt.com/zmod4410.

About IDT

Integrated Device Technology, Inc., a wholly owned subsidiary of Renesas Electronics Corporation (TSE: 6723), develops system-level solutions that optimize its customers’ applications. IDT’s market-leading products in RF, high performance timing, memory interface, real-time interconnect, optical interconnect, wireless power and smart sensors are among the company’s broad array of complete mixed-signal solutions for the communications, computing, consumer, automotive and industrial segments. Headquartered in San Jose, Calif., IDT has design, manufacturing, sales facilities and distribution partners throughout the world. Additional information about IDT can be found at www.IDT.com. Follow us on Facebook, LinkedIn, Twitter, and YouTube.

###

©2019, Integrated Device Technology, Inc. IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc., and its worldwide subsidiaries. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.

この記事をシェアする