メインコンテンツに移動

IDT to Showcase Video Transcoding Innovations at NAB 2018

2018年4月9日

SAN JOSE, Calif., April 9, 2018 – Integrated Device Technology, Inc. (IDT) (NASDAQ: IDTI) will demonstrate to attendees of NAB 2018, the top technology event for the media and entertainment industry, how its latest HEVC and AVC compression solutions address service providers and OTT operators’ critical requirements for higher densities and lower costs to support cloud video applications. Live demonstrations will be at IDT’s meeting room, SU11324MR, in South Upper Hall, Las Vegas Convention Center, April 9 to 12, 2018.

One of the key demonstrations will be of the IDT® R22-GPU HEVC software encoder, an ideal solution for the next generation of high-efficiency video delivery. The highly scalable architecture of the R22-GPU software encoder is designed for distributed HEVC encoding on hybrid x86 platforms with integrated GPUs. The demonstration at NAB will showcase real-time high quality 4Kp60 10-bit HDR HEVC transcoding on a COTS server platform. 

HEVC transcoding based on the IDT® R22-GPU software offers many advanced features, including:

  • High-quality, real-time 10-bit HEVC up to 4Kp60 leveraging GPU acceleration and IDT’s leading video compression expertise
  • Broadcast quality 4K video with 10-bit HDR support
  • Integration with FFmpeg framework for easy application development and integration into private and public cloud workflows

IDT will also showcase the latest release of the IDT® R12-CPU, a premium quality H.264/AVC software transcoder optimized for broadcast, adaptive bitrate OTT video and cloud video transcoding services.  IDT will demonstrate how R12-CPU can reduce operators and service providers’ costs by up to 40% over their current workflow.  R12-CPU is available for evaluation and production use and is widely deployed by content and service providers worldwide.

“The latest solutions we will demonstrate at NAB 2018 showcase our ongoing commitment to enabling highest quality video solutions with outstanding TCO per channel that media and entertainment providers require,” said David Ko, senior manager of product marketing, OID Video Product Line.

To schedule a meeting with IDT at the show, please contact [email protected].

About IDT

Integrated Device Technology, Inc. develops system-level solutions that optimize its customers’ applications. IDT’s market-leading products in Video Compression, RF, high performance timing, memory interface, real-time interconnect, optical interconnect, wireless power, and smart sensors are among the company’s broad array of complete mixed-signal solutions for the broadcast, communications, computing, consumer, automotive and industrial segments. Headquartered in San Jose, Calif., IDT has design, manufacturing, sales facilities and distribution partners throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT can be found at www.IDT.com. Follow IDT on Facebook, LinkedIn, Twitter, and YouTube.

###

© 2018, Integrated Device Technology, Inc. IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc., and its worldwide subsidiaries. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.

この記事をシェアする