SANTA CLARA, Calif., May 17, 2011 — NEC LCD Technologies (NLT), Ltd., together with Renesas Electronics America Inc., its sales and marketing channel in the Americas, today introduced two new transflective color thin film transistor (TFT) LCD modules for industrial applications and applications requiring indoor and outdoor viewability. The display modules, 6.5-inch SVGA (800 x 600) (part number NL8060BC16-01) and 10.4-inch XGA (1024 x 768) (part number NL10276BC20-10), incorporate NLT's proprietary super-reflective natural light TFT (SR-NLT) technology resulting in displays operable in both transmissive mode (using a backlight) and reflective mode (using available ambient light). The displays are targeted for use in portable medical systems used in the field and in a hospital or clinic setting, in industrial equipment and in other indoor/outdoor display applications. Both the 6.5-inch and 10.4-inch modules will be on display in Renesas Electronics America's booth (#835) at Society of Information Display (SID) 2011 in the Los Angeles Convention Center, May 17-19.
NEC LCD Technologies' proprietary SR-NLT technology enhances LCD viewability in outdoor lighting environments. In the reflective mode, the display module capitalizes on NEC’s optimized LCD panel design to provide excellent visibility, even in outdoor daylight conditions. The displays also incorporate an eco-friendly LED backlight system that results in lower power consumption. Since images on the display are readable when the backlight is turned off, power consumption can be further reduced.
"While NLT has historically used its SR-NLT technology in a variety of small-size LCDs (4.X-inch and below), the new 6.5-inch and the 10.4-inch modules are the first mid- and large-size SR-NLT LCD modules to go to mass production," said Dr. Shigehiko Satoh, Vice President, Display Business Unit, Renesas Electronics America. "These products, featuring an LED backlight system, a 35 percent reflection ratio and a 15:1 contrast ratio when the backlight is turned off, offer customers a display that is viewable in both high- and low-ambient light environments."
Additional Product Features
Features | NL8060BC16-01 | NL10276BC20-10 |
---|---|---|
Size/Resolution | 6.5-inch SVGA (800 x 600) | 10.4-inch XGA (1024 x 768) |
Brightness | 300 cd/m2 | 175 cd/m2 |
Contrast Ratio | 150:1 (on), 15:1 (off) | 150:1 (on), 15:1 (off) |
Reflection Ratio | 35٪ | 35٪ |
Color Gamut | 40٪ (on) | 40٪ (on) |
Power of Backlight | 3.7W | 4.66W |
Input Signal | LVDS (6/8-bit) | LVDS (6/8-bit) |
Availability | Now | Now |
Renesas at SID 2011
Renesas Electronics America in conjunction with NEC LCD Technologies will showcase a full lineup of innovative LCD technologies during Society for Information Display’s Display Week, May 17-19, at the Los Angeles Convention Center. Throughout the week in booth #835, the companies will highlight more than 30 LCD modules, ranging from 3.5 inches to 21.3 inches, optimized for a variety of applications, including industrial/test and measurement, medical and gaming systems, and emerging segments such as 3D, touch panel and color enhancements.
Representatives from NEC LCD Technologies will present three poster presentations on Thursday, May 19, from 4:00 to 7:00 p.m. in the West Exhibit Hall B of the Los Angeles Convention Center. Topics include:
- A High-Resolution Multi-View 2D/3D Display with HxDP Arrangement and Its Optical Characterization, by Koji Shigemura
- Analysis of Temperature Dependence of 3D Viewing Space for Autostereoscopic Display, by Wu Di
- Novel Lenticular-Lens Fabrication Method on Glass by Using Ink-Jet Printer, by Jin Matsushima
About Renesas Electronics America’s Display Business
Renesas Electronics America is the exclusive representative in the Americas of NEC LCD Technologies, a leading supplier of innovative LCD products for industrial applications. With an extensive lineup of 2.7- to 22.5-inch AM-LCD modules and a network of distributors and value-added partners (VAPs), Renesas Electronics America provides complete display module solutions from NEC LCD Technologies to the industrial, medical and high-end monitor market. In addition to modules based on NEC LCD Technologies' SFT for ultra-wide viewing, Renesas Electronics America also offers LCD modules that include ultra-high resolutions, wide temperature ranges, high contrast ratios, rich color gamuts, backward compatibility, LED backlights, and transflective viewing for use in diverse lighting environments.
Renesas Electronics America and NEC LCD Technologies are committed to delivering innovative, high-performance, eco-conscious LCD solutions that address the diverse size, power and high image-quality needs of their industrial, medical and high-end monitor customers. Based on technologies developed by NEC LCD Technologies, the LCD modules are optimized and designed for a range of applications, including portable and fixed medical equipment, test and measurement devices, instrumentation equipment, point-of-sale systems, gaming systems, global positioning systems, radio-frequency identification devices and barcode scanners.
Additional information about these LCD display products, manufactured by NEC LCD Technologies and exclusively represented by Renesas Electronics America in the Americas, can be found at http://www.nec-lcd-am.com/.
About Renesas Electronics America Inc.
Renesas Electronics America Inc., headquartered in Santa Clara, California, is a wholly owned subsidiary of Renesas Electronics Corporation (TSE: 6723), the world's number one supplier of microcontrollers and a premier supplier of advanced semiconductor solutions including microcontrollers, SoC solutions, and a broad range of analog and power devices. In the Americas, Renesas Electronics America markets and sells industrial-type active-matrix LCD modules from NEC LCD Technologies, Ltd., a global leader in innovative display technologies. More information about the products offered by Renesas Electronics America can be found at www.renesas.com.
The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.