KAWASAKI, JAPAN, SANTA CLARA, Calif., DUSSELDORF, Germany, September 27, 2013 — NLT Technologies (NLT), together with its sales and marketing channels in the Americas and Europe, Renesas Electronics America, Inc. and Renesas Electronics Europe GmbH, today announced development of four new amorphous-silicon thin-film-transistor (TFT) liquid crystal display (LCD) modules. These modules are ideal for outdoor applications used boating equipment or construction devices.
The new wide format TFT LCD modules are well suited for use in industrial display applications. They are equipped with long-life white LED backlight units that achieve high luminance and also contribute to lower maintenance costs for equipment and reduced environmental impact.
Size / Resolution | Part Number | Remarks |
---|---|---|
7.0 inch / WVGA | NL8048AC19-13 | Long life time of 100,0000 hours |
7.0 inch / WVGA | NL8048AC19-14F | 1000cd/㎡, Long life time of 100,000 hours |
8.0 inch / WVGA | NL8048AC21-01F | 1000cd/㎡, Long life time of 100,000 hours |
12.1 inch / WXGA | NL12880BC20-07F | 1500cd/㎡ |
Samples of these products are scheduled to be available in October 2013.
The main characteristics of the new modules are as follows:
1) Ultra high luminance
The 7.0 inch NL8048AC19-14F and 8.0 inch NL8048AC21-01F have a luminance of 1000cd/m2, and the 12.1 inch NL12880BC20-07F has a luminance of 1500 cd/m2 resulting in excellent viewability even in high ambient light environments. The displays are ideal for display applications in outdoor environments.
2) Long-life LED backlight
The long-life LED backlights used in the new 7-inch and 8-inch WVGA modules have an estimated life span of 100,000 hours – equivalent to almost 12 years of continual usage. This results in easy, low cost maintenance for these displays.
Adoption of the white LED backlight results in lower environmental impact since the backlights consume limited power and are mercury free.
The 12.1-inch, NL12880BC20-07F, utilizes NLT’s proprietary color reproduction technology, ColorXcell, which enables vivid color reproduction of images without increasing power consumption. Use of an LED backlight in combination with NLT’s ColorXcell technology achieves further reduction of power consumption.
3) Wide operating temperature range
All four of the new modules feature wide operating temperature ranges. The 7.0-inch WVGA and 8.0-inch WVGA modules have an operating temperature range of -30 to +80 degrees C, and the 12.1-inch NL12880BC20-07F -20 to +70 degrees C. The wide operating ranges of these displays guarantees stable operation even in very low and very high temperature environments.
Typically displays used in outdoor environments are equipped with high power backlights in order to achieve sufficient viewability when exposed to strong light such as direct sunlight. Under these conditions LED backlights tend to require greater power consumption in order to achieve sufficient luminance to be seen in outdoor settings, this in turn shortens a backlight’s lifespan. Achieving longer backlight lifespan and reducing maintenance costs of outdoor display equipment has, therefore, been a challenge. The newly introduced LCD modules by NLT Technologies respond to this market demand by achieving the long lifespan of white LED backlights while achieving high luminance by optimizing the heat dissipation performance of the backlight.
NLT Technologies continues to invest and develop high image quality and high reliability LCD modules to meet the various demands of industrial display applications, which will contribute to the adoption of LCDs in more industrial applications.
These new LCD modules will be showcased in NLT Technologies’ booth # 2B01 at CEATEC JAPAN 2013, which is being held from October 1 to 5 in Makuhari Messe, Japan.
Main specifications of the new LCD modules can be found in the attachment
About Renesas Electronics Europe’s Display Business
Renesas Electronics Europe is the authorized representative in Europe of NLT Technologies, Ltd. (established July 2011 as a joint venture between NEC Corporation and Shenzen AVIC Optoelectronics, Ltd.), a leading supplier of innovative LCD products for industrial applications. With an extensive lineup of 3.5- to 22.5-inch active-matrix LCD modules and a network of distributors, Renesas Electronics Europe provides complete display module solutions from NLT Technologies to the industrial, medical and high-end monitor market. In addition to modules based on NLT Technologies' SFT for ultra-wide viewing, Renesas Electronics Europe also offers LCD modules that include ultra-high resolutions, wide temperature ranges, high contrast ratios, rich color gamuts, backward compatibility, LED backlights, and transflective viewing for use in diverse lighting environments.
Renesas Electronics Europe and NLT Technologies are committed to delivering innovative, high-performance, eco-conscious LCD solutions that address the diverse size, power and high image-quality needs of their industrial, medical and high-end monitor customers. Based on technologies developed by NLT Technologies, the LCD modules are optimized and designed for a range of applications, including portable and fixed medical equipment, test and measurement devices, instrumentation equipment, point-of-sale systems, gaming systems, global positioning systems, factory automation and barcode scanners.
Additional information about these LCD display products, manufactured by NLT Technologies and represented by Renesas Electronics can be found at www.renesas.eu/display
The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.