メインコンテンツに移動

Renesas Electronics America and Cogent Computer Systems Introduce a Highly Integrated Renesas SH-Mobile SH7724 SODIMM System-On-Module (SOM) for Embedded Systems

System Engineers Building Embedded Systems Using Renesas Electronics’ SH7724 Microprocessor Can Easily Implement Their Embedded System Products by Utilizing the Turnkey SOM

2011年5月4日

SANTA CLARA, Calif. and SMITHFIELD, Rhode Island, May 4, 2011-Renesas Electronics America Inc. and Cogent Computer Systems Inc. announced today the availability of the CSB765 - Renesas SH-Mobile SH7724 System On Module (SOM), which provides low cost and enables rapid development of systems incorporating the SH-Mobile SH7724 application processor for embedded systems.

Product Background

The SH-Mobile R-Series is an application processor based on Renesas SH-Mobile series, which is widely used in mobile phones in Japan and other countries. It was developed to allow advanced multimedia functions of the SH-Mobile device such as camera processing, and video and audio processing, to be applied in fields other than mobile phones. The processor incorporates multi-codec, high-performance video processing IP supporting the H.264/MPEG-4 AVC (H.264) video compression standard used by ISDB-T terrestrial digital broadcasts in Japan, as well as the One-Seg format used for terrestrial digital broadcasts in Europe, China and other regions. To support playback and recording of HD (high definition, 1280 x 720 pixels) video, functionality is provided for encoding (recording) and decoding (playback) of HD-format video at 30 frames per second (fps). Also, the operating frequency of 500 megahertz (MHz) provides power to spare when running a general-purpose operating system (OS) such as Linux.

In addition to the these features, camera input has been increased to two channels and an Ethernet MAC (Media Access Control) supporting data transfer at 10/100 megabits per seconds (Mbps) has been newly added. This extends the range of suitable applications beyond low-end navigation systems, where Renesas Electronics' application processors already have an extensive track record, to include IP security cameras, videoconferencing systems, video and voice over IP (V2IP), networked household appliances, drive recorders, digital signage, etc.

Cogent’s CSB765 SOM Features

Cogent delivers sophisticated boards that are small in size and price, fully featured and easy to use. A Cogent CSB765 SOM provides more time, at less cost and less risk, for engineers to create their unique products, based on the proven Renesas Electronics SH-Mobile SH7724 applications processor.

The GPIO and peripherals are made available via the low cost 200-pin SODIMM edge connector. Ultra small size, a high-performance 500Mhz superscalar SH-4A core, a double-precision FPU, multiple serial interfaces, generous memory, 10/100 Ethernet and on-board 3.3 volt (V) regulator all combine to make the CSB765 SOM an excellent choice for any size-restricted, low-power embedded system. In addition, the on-chip hardware video decoding, 2D graphics engine, audio DSP and video input allow the CSB765 SOM to target highly sophisticated multimedia and video-streaming applications.

Specifications

  • 500MHz SH-4A superscalar core (900 DMIPS) with 32 KB I-cache/32 KB D-cache
  • 256KB L2 cache and 128KB on-chip high-speed media SRAM
  • IEEE754-compliant single-/double-precision FPU (3.5GFLOPS)
  • 128MB low-power mobile LPDDR-333 SDRAM
  • 64MB S29GL512N flash, with secure 256 byte sector and 128-bit unique ID
  • On-chip LCD controller up to 1280 x 720 pixels with 2D graphics, scaling and rotation
  • Hardware video decoding up to 720P, MPEG-4, H.264, JPEG and WMV
  • 8-bit video-input port supporting YUV4:2:2, CCIR656 and CMOS sensors up to 5MP
  • Sound processing unit with dual 24-bit MAC DSP, 160KB program and 264KB data RAM
  • High-speed (480MBit) USB 2.0 OTG port and USB host port
  • On-chip 10/100Mbit Ethernet controller
  • DS1339 real-time clock with dedicated battery backup input
  • 2-wire RS-232 debug serial port plus three 2-wire TTL UARTS (with GPIO handshaking)
  • I2S, SPI (x2) and I2C (x2) for I/O expansion such as touch, audio, A/D, D/A, etc.
  • Dual SD/MMC controllers (4-bit, SDIO-compliant)
  • Buffered 25-bit address/16-bit data bus for generic expansion
  • 10 dedicated GPIO (may also carry some CPU functions)
  • On-board, wide input (6V to 24V) 3.3V regulator provides 3A to the target board
  • <750mw typical, 1500mw maximum, <20mw sleep to RAM

Pricing and Availability

More information about the CSB765 SOM can be found at www.cogcomp.com/csb_csb765.htm. For pricing and availability, contact NuHorizons http://www.nuhorizons.com/.

About Renesas Electronics America Inc.

Renesas Electronics America Inc., headquartered in Santa Clara, California, is a wholly owned subsidiary of Renesas Electronics Corporation (TSE: 6723), the world's number one supplier of microcontrollers and a premier supplier of advanced semiconductor solutions including microcontrollers, SoC solutions, and a broad range of analog and power devices. Renesas Electronics America offers local manufacturing in Roseville, California, and the global manufacturing capabilities of its parent company. In the Americas, Renesas Electronics America markets and sells industrial-type active-matrix LCD modules from NEC LCD Technologies, Ltd., a global leader in innovative display technologies. More information about the products offered by Renesas Electronics America can be found at www.renesas.com.

About Cogent Computer Systems, Inc.

Cogent Computer Systems, Inc. (www.cogcomp.com) has been designing and manufacturing System On Module (SOM) Computers since 1992. All products are produced in our state of the art, IPC-610 Class 3 facility located in Smithfield, R.I. Cogent also offers hardware design services as well as licensing of our SOM designs for high-volume off-shore manufacturing.

Based upon today's most popular integrated CPU architectures, Cogent’s SOMs are small in size and price, fully featured and easy to use. The CSB7xx-series SOMs provides a cost-effective platform for low-power CPUs. CSB17xx series SOMs are oriented for high-performance networking and multimedia applications with PCI Express®, Gigabit Ethernet, Serial ATA and HDMI Video output. While our boards derive much of their functionality from the CPU, we supplement that functionality with carefully selected peripherals, memory and power.

PCI Express is a registered trademark of PCI-SIG.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

この記事をシェアする