メインコンテンツに移動

Renesas Electronics Announces Low-Loss Silicon Carbide (SiC) Power Devices Integrating Power Conversion Circuit in Single Chip

Contribute to Better Power Efficiency in High-Output Electronic Systems such as Air Conditioners, Communication Base Stations, and Solar Power Arrays

2012年1月17日

TOKYO, Japan, January 17, 2012 — Renesas Electronics Corporation (TSE: 6723), a premier provider of advanced semiconductor solutions, today announced the development of a Schottky barrier diode (SBD), the RJS6005TDPP, employing silicon carbide (SiC, Note 1), a material considered to have great potential for use in power semiconductor devices. The new SiC Schottky barrier diode is ideal for use in high-output electronic systems such as air conditioners, communication base stations, and solar power arrays. The new device also incorporates technology developed jointly by Hitachi, Ltd., and Renesas Electronics, which contributed to achieving approximately 40 percent reduced low power consumption compared to Renesas Electronics' existing power devices employing conventional silicon (Si).

Recently, demand has grown for more highly efficient power supply circuits in many types of systems to promote environmental preservation. There is particularly strong demand for more efficient power conversion in products using power switching circuits or inverter circuits enabling precise motor control, such as air conditioners, communication base stations, PC servers, and solar power arrays. Therefore, the diodes used in these power converter circuits need to provide faster switching speeds and low-voltage operation. Renesas Electronics developed the new SiC SBD to address these demands.

Key features of the new RJS6005TDPP SiC SBD:

(1) Faster switching speed for 40 percent lower loss than existing products

The new RJS6005TDPP SiC SBD has a reverse recovery time (Note 2) of 15 nanoseconds (standard value: measuring conditions IF = 15 A, di/dt = 300 A/µs), approximately 40 percent faster than that of existing Renesas Electronics products employing silicon. This enables a faster switching speed and reduces power loss by approximately 40 percent compared with Renesas Electronics' Si-based products.

In addition, the reverse recovery time does not degrade when the temperature rises, enabling consistently low switching loss when operating in high-temperature environments.

(2) Low-voltage operation

The new SiC-SBD has a voltage rating (forward voltage, VF) of only 1.5 volts (V), lower than that of existing Si fast trigger diode products. In addition, the temperature dependency of this characteristic is small, ensuring that a stable forward voltage can be obtained even under high-temperature conditions. This means that more compact heat dispersion measures can be used.

The new RJS6005TDPP SiC-SBD uses a package equivalent to the industry-standard fully-molded TO-220, with which it is also pin compatible. This means that the RJS6005TDPP SiC SBD can easily be used as a replacement for conventional silicon diodes on existing printed wiring boards.

Renesas Electronics has a lineup of 3 ampere (A) to 30 A, voltage tolerance 600 V, power devices designed to meet the need for better energy efficiency in high-output systems such as air conditioners, communication base stations, and solar power arrays, and plans call for the introduction of a series with a voltage tolerance of 1,200 V. Renesas Electronics aims to provide customers with total solutions combining MCUs and Analog & Power devices, and also to become the leading power device supplier. The company plans to enhance its kit solutions and compound semiconductor devices, with the new high-voltage SiC-SBD power devices at the core, supplemented by peripheral power supply control ICs, high-performance IGBTs, high-voltage super-junction MOSFETs, and photocouplers.

Please refer to the separate sheet for the specifications of the new RJS6005TDPP SiC SBD.

Pricing and Availability

Samples of Renesas' new RJS6005TDPP SiC SBD is available now, priced at US$5 per unit. Mass production is scheduled to begin in March 2012 and is expected to reach a volume of 100,000 units per month with August 2012. (Pricing and availability are subject to change without notice.)

(Note 1) Silicon carbide (SiC):
A material that exceeds silicon in characteristics such as thermal conductivity, permissible operating temperature, radiation exposure, and insulation breakdown field strength, giving it great potential for use in low-loss power devices.

(Note 2) Reverse recovery time:
When a diode switches from the on to the off state after the prescribed forward current has been flowing through it, reverse current flow occurs due to a small number of carriers accumulated in the junction. The reverse recovery time expresses the amount of time required to recover to the prescribed current value after the switch to the off state.

(Remarks) All other registered trademarks or trademarks are the property of their respective owners.

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

この記事をシェアする