メインコンテンツに移動

Renesas Electronics Europe Announces New High-Speed Optocouplers Offering Extended Operating Temperature Range Combined with High Isolation and Shielding Features

2012年2月9日

Dusseldorf, February 9, 2012 — Renesas Electronics Europe, a premier supplier of advanced semiconductor solutions, today announced the availability of two new high-performance optocouplers, the PS9324 and the PS9123, for industrial and motor control applications. The new high-speed optocouplers are designed for 10 megabits per second (Mbps) high-speed operation over an extended temperature range: between -40°C and 100°C for the PS9123 series and up to 110°C for the PS9324 series. The new devices comply with international safety standards such as UL, CSA and VDE (optional), making them ideally suited for applications in harsh industrial environments such as factory automation (FA), measurement equipment and motor-control.

Optocouplers are electronic components capable of electrically insulating an input signal from an output signal. In the same package, they contain an electrically insulated light-emitting diode (LED) that converts an electrical signal into light, and an electrically insulated photo-detect device that converts the light back into an electrical signal.

The PS9324 series and PS9123 series are optically-coupled high-speed isolators containing a a gallium-aluminum-arsenide (GaAlAs) LED on the input side and a photodiode and a signal processing circuit on the output side on one chip. The detector IC of the active low type PS9324 series features an open collector output and low operation voltages from 2.7V to 5.5V, allowing flexible circuit design. A communication speed of 10Mbps can be achieved due to the specified maximum propagation delay times of 75 nanoseconds (ns) at 25°C and typical values of 40 ns.

The PS9123 series comes with a totem pole output, offering shorter propagation delay times as low as 65ns (max) at 25°C. The maximum pulse width distortion |tPHL - tPLH| is less than 35 ns for the PS9324 series and less than 50 ns for the PS9123 series.

For operation in noisy industrial environments Renesas’ new optocouplers have an internal shield providing a common-mode transient immunity (CMTI) of minimum 15kV/µs and typical values of 20kV/µs. The PS9324 comes in a in a small 6-pin shrink dual inline package (SDIP). The small package reduces the mounting space by 50 percent compared to a classical 8-pin DIP package while guaranteeing the highest isolation voltage of 5kVrms and achieving a minimum creepage distance of 8mm (PS9324L2).

The PS9123 is delivered in a 5-pin small outline package (SOP), with a minimum pin-to-pin distance of 1.27mm, allowing space saving designs.

Availability

Samples of Renesas’ new PS9324 and PS9123 series of optocouplers are available now. Mass production is scheduled to begin in February 2012. Availability is subject to change without notice.

(Remarks) All names of products or services mentioned in this press release are trademarks or registered trademarks of their respective owners.

About Renesas Electronics Europe

Renesas delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live – securely and safely. As the number one global supplier of microcontrollers, and a leader in A&P and SoC products, Renesas provides the expertise, quality, and comprehensive solutions for a broad range of Automotive, Industrial, Home Electronics (HE), Office Automation (OA) and Information Communication Technology (ICT) applications to help shape a limitless future.

Renesas Electronics Corporation was established in 2010 and is headquartered in Japan.With over 800 hardware and software alliance partners worldwide, it has the industry’s largest local support network. Renesas Electronics’ European structure is comprised of three business units – the Automotive, the Broad-based and the Industrial Solution Business Unit.

Further information about Renesas Electronics Europe is available at www.renesas.com

Renesas Electronics Europe is also on social media at http://twitter.com/Renesas_Europe, http://facebook.com/RenesasEurope and http://youtube.com/RenesasPresents.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

この記事をシェアする