メインコンテンツに移動

Renesas Electronics supports HIPERFACE DSL® Digital Encoder Interface with RZ/T1 Solution

RZ/T1 Group of MPUs Delivers Real-Time Operation for High-Precision AC Servo Applications

2017年11月7日

TOKYO, Japan, November 7, 2017 – Renesas Electronics Corporation (TSE: 6723), a premier supplier of advanced semiconductor solutions, today announced a new solution package for its RZ/T1 Group of microprocessors (MPUs) supporting HIPERFACE DSL® digital encoder interface for AC servo applications. The support of HIPERFACE DSL for RZ/T1 reduces the customer’s system bill-of-materials (BOM) cost and enables faster time-to-market.

The RZ/T1 Group includes the Arm® Cortex®-R4 processor with a dual precision floating-point unit (FPU) operating at up to 600 megahertz (MHz), and provides: real-time processing, tightly-coupled memory, high-speed analog to support dual servo motors, and network connectivity for distributed motion that matches the needs of precise AC servo drive applications.

The RZ/T1 already supports other leading encoder interfaces including EnDat 2.2, BiSS®-C, Tamagawa and A-formatTM. This time, the RZ/T1 newly supports the HIPERFACE DSL digital encoder interface. These digital, bidirectional interfaces provide precise position values from absolute encoders. Instead of using a separate FPGA or ASIC, integrating these encoder interfaces on the RZ/T1 reduces the component count and cuts system costs.

With this expanded functionality, the RZ/T1 now supports most of the leading encoder interfaces, and with its unique configurable encoder interface, it simplifies swapping different encoders interfaces from a single device platform. 

HIPERFACE DSL® is an industry-leading interface provided by SICK STEGMANN GmbH, and uses the familiar RS485 cabling with a transmission rate of 9.375 mega baud rate. The data is transmitted in synchronization with the drive cycle, and the cable between the drive electronic and feedback system can be up to 100 meters in length.

Key features of the solution package:

The solution package for HIPERFACE DSL provides all required support to connect the RZ/T1 to corresponding slave devices:

  1. Encoder interface configuration data: programs the configurable encoder interface to operate in HIPERFACE DSL mode and to be able to connect to a corresponding slave device
  2. Sample driver code: enables the application program to communicate with the encoder through a simple API
  3. Documentation: API and example program descriptions are provided in an application note; a user’s manual for the HIPERFACE DSL encoder enables individual modifications and extensions of the given code samples

“The availability of HIPERFACE DSL for the RZ/T1 proliferates the adoption of our powerful encoder technology in the market,” said Clemens Bitsch, Product Manager of HIPERFACE DSL, SICK STEGMANN GmbH. “We see the digital encoder evolution as a substantial driver for efficient and cost-optimized systems and as a pre-requisite for the Industry 4.0.”

As a solution provider, Renesas, in collaboration with partners, is committed to providing AC servo solutions that support innovative and future-proven system architectures.

Availability

The HIPERFACE DSL solution package for RZ/T1 will be available in December 2017. Renesas will showcase the solution package combined with the RZ/T1 at the Renesas booth (Hall 10.1, Stand 130) at SPS IPC Drives exhibition to be held in Nuremberg, Germany from Nov 28 to 30, 2017.

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power, and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.

(Remarks) HIPERFACE DSL is registered trademark of SICK STEGMANN GmbH, EnDat is registered trademark of DR. JOHANNES HEIDENHAIN GmbH, BiSS is registered trademark of iC-Haus GmbH, A-format is a trademark of Nikon Corporation, Arm and Cortex are registered trademarks or trademarks of Arm Limited. Registered trademarks or trademarks are the property of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

この記事をシェアする