Registration is Now Open for the Unique Running Sport that Splits a 15K Race into 2 Legs

2015年7月30日

SAN JOSE, Calif., July 30, 2015 – Integrated Device Technology, Inc. (IDT®) (NASDAQ: IDTI) announced today that registration is open for the Double Racing Festival’s return to San Jose on Aug. 22. The centerpiece of the unique family-friendly festival is the Double Road Race 15K, which splits the race into two legs—a 10K and a 5K, with a break in between. The race was developed by Bob Anderson, founder of Runner’s World magazine.

The race begins and ends at the headquarters of IDT, the presenting sponsor of the San Jose event. Times from the two legs are combined for scoring.

The festival will feature live music and food. In addition to the Double Road Race, two additional racing events are scheduled at the festival. The UjENA Double 5K features a 3K leg and a 2K leg. Children 13 and younger can participate in the 1.5-mile Kids Cup Double, with a 1-mile leg followed by a half-mile leg. All races include a halftime. All Double Road Race finishers receive a medal, official race T-shirt, and a draw-string tote bag.

“This festival is a great family event, and IDT is proud to be the presenting sponsor once again,” said Leslie Garcia of IDT. “Whether you’re competing for first place or simply challenging yourself to cross the finish line, the Double Racing Festival has something for folks of all ages and capabilities.”

For more information about the race and to register, visit www.SanJoseDouble.com.  IDT headquarters is located at 6024 Silver Creek Valley Road.

About IDT

Integrated Device Technology, Inc. develops system-level solutions that optimize its customers’ applications. IDT uses its market leadership in timing, serial switching and interfaces, and adds analog and system expertise to provide complete application-optimized, mixed-signal solutions for the communications, computing and consumer segments. Headquartered in San Jose, Calif., IDT has design, manufacturing, sales facilities and distribution partners throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com. Follow IDT on Facebook, LinkedIn, Twitter, YouTube and Google+.

IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.

この記事をシェアする