メインコンテンツに移動

Transphorm Announces Low-Cost Driver Solution for SuperGaN FETs

Transphorm FETs Deliver Up to 99% Efficiency Using Simple Half-Bridge Gate Driver, Validating Cost-Effective Design Option for a Wide Power Range Exceeding One Kilowatt

2023年6月8日

GOLETA, Calif.——Transphorm, Inc. (Nasdaq: TGAN)—a global leader in GaN, the future of next generation power systems—released details on a high-performance, . For use in low- to mid-power applications such as LED lighting, charging, microinverters, UPSes, and gaming computers, the design option strengthens the company's value proposition for customers in those segments of the $3 billion power market.

Unlike competing e-mode GaN solutions that require custom drivers or level shifting circuitry with gate protection devices, Transphorm's SuperGaN® FETs are known for easy drivability given they pair with off-the-shelf drivers. This capability adds to the cost advantages customers gain when using Transphorm devices. The newly defined solution uses a high-speed, non-isolated, high-voltage half-bridge gate driver that further reduces total system cost without affecting the GaN FET's or system's performance.

"Our normally-off GaN platform is preferable given its ability to work with well-known off-the-shelf drivers. The ability to use a select driver is a major advantage. It allows customers to choose drivers based on varying degrees of performance benefits while retaining more control over the power system's cost. This is particularly important for price sensitive end markets," said Philip Zuk, Senior Vice President, Business Development and Marketing, Transphorm. "With Transphorm's devices that deliver fundamentally higher performance, customers can build a BOM based on the end result they need, reaching the required performance as cost-effectively as possible."

Transphorm also recommends various other drivers that feature high isolation voltage ratings (control-to-output drive signals), short propagation delay times, fast turn on/off times, and programmable deadtime among other advantages—making them well-suited for higher power applications.

Low- to mid-power applications such as power adapters, gaming laptop chargers, LED lighting, and two- and three-wheeler chargers are price sensitive. The power systems in these types of products do not typically require advanced features like safety isolation. Therefore, using premium drivers may unnecessarily increase the cost of the bill of materials (BOM).

Performance Analysis

The half-bridge gate driver was tested with the TP65H070LSG, Transphorm's 650 V, 72 mΩ device in a PQFN88 package. It can be used in bridge topologies such as resonant half-bridge, totem-pole PFC, sine-wave inverter, or active clamp flyback.

Test results show that the low-cost driver solution performs well at switching frequencies that are less than/equal to 150 kHz with or without the use of a heatsink or forced air for cooling. The solution ultimately achieved close to 99 percent efficiency in select configurations.

Application Note Access

For more details about the above solution, download the AN0014 application note titled Low Cost, High Density, High Voltage Silicon Driver for Low- to Mid-Power GaN FET Applications here: .

About Transphorm

Transphorm, Inc., a global leader in the GaN revolution, designs and manufactures high performance and high reliability GaN semiconductors for high voltage power conversion applications. Having one of the largest Power GaN IP portfolios of more than 1,000 owned or licensed patents, Transphorm produces the industry's first JEDEC and AEC-Q101 qualified high voltage GaN semiconductor devices. The Company's vertically integrated device business model allows for innovation at every development stage: design, fabrication, device, and application support. Transphorm's innovations move power electronics beyond the limitations of silicon to achieve over 99% efficiency, 50% more power density and 20% lower system cost. Transphorm is headquartered in Goleta, California and has manufacturing operations in Goleta and Aizu, Japan. For more information, please visit www.transphormusa.com. Follow us on Twitter @transphormusa and WeChat @ Transphorm_GaN.

The SuperGaN mark is a registered trademark of Transphorm, Inc. All other trademarks are the property of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

この記事をシェアする