メインコンテンツに移動

Transphorm Releases Compact 240W Power Adapter Reference Design with Industry's Only High Performance TO-220 GaN FETs

Industry-Standard Thru-hole Packaging Not Offered by Competing GaN Technology Brings Power Density Advantages at Low Cost to Power Supplies

2023年1月5日

GOLETA, Calif. — Transphorm, Inc. (Nasdaq: TGAN)—a pioneer in and global supplier of high reliability, high performance gallium nitride (GaN) power conversion products—today announced availability of its new 240W Power Adapter Reference Design. The TDAIO-TPH-ON-240W-RD deploys a CCM Boost PFC + Half-Bridge LLC topology to deliver a peak power efficiency of over 96 percent with a power density up to 30 W/in3. Transphorm's design uses three SuperGaN® FETs (TP65H150G4PS) each with an on-resistance of 150 milliohms. The GaN FET comes as a 3-lead TO-220, a well-known and long-trusted transistor package that offers superior thermals at lowline for higher current power systems running PFC configurations.

The reference design is intended to simplify and quicken power system development for applications such as high-power density AC-to-DC power supplies, fast chargers, IoT devices, laptops, medical power supplies, and power tools.

Key Specifications and Features

The TDAIO-TPH-ON-240W-RD is a 240W 24V 10A AC-to-DC power adapter reference design. It pairs the TP65H150G4PS GaN FETs with onsemi's off-the-shelf NCP1654 CCM PFC controller and NCP1399 LLC controller. The design uses a 25 millimeter heatsink that produces a power density of over 24 W/in3. The power density can increase by approximately 25 percent to 30 W/in3 depending on the heatsink design.

This high power density and efficiency range is primarily due to the FET's packaging as Transphorm offers the only high voltage GaN devices in a TO-220 today. Power adapters, along with all universal AC-to-DC power supplies, require high current at lowline (i.e., 90 Vac) which can require paralleling two PQFN packages (as typically seen with e-mode GaN) to achieve the desired power output. This method reduces a power supply's power density while requiring 2x part count. Transphorm's TO-220 packages mitigate this, thus providing unparalleled power density at a lower cost—a result not currently possible with e-mode GaN.

Other specifications and features include:

  • Operation over universal input voltage of 90 to 264 Vac
  • Over 96% peak efficiency and flat efficiency curve across line and load
  • Tight switching frequency regulation for improved input EMI filter utilization
  • Over 180 kHz switching frequency operation for compact implementation

The new reference design joins a broad portfolio of adapter/fast charger design tools offered by Transphorm. That portfolio currently includes five open frame USB-C PD reference designs ranging from 45 to 100 watts. It also includes two open frame USB-C PD/PPS reference designs for 65W and 140W adapters.

SuperGaN® Technology Difference

When designing its SuperGaN platform, Transphorm's engineering team drew on learnings from production ramps of previous products and paired that knowledge with its drive for performance, manufacturability, and cost improvements. The result was a new GaN platform comprised of patented technology offering ultimate simplicity and substantial improvements in various areas, such as:

  • Performance: a flatter, higher efficiency curve with an improved Figure of Merit (RON*QOSS) of ~10 percent
  • Designability: elimination of a switching node snubber requirement at high operation currents.
  • Cost: simplification of device assembly helps reduce cost.
  • Robustness: industry leading gate robustness of +/- 20 Vmax and noise immunity of 4 V.
  • Reliability: industry leading reliability with a < 0.10 FIT rate with 85B+ hours of field operation.

Availability

The TDAIO-TPH-ON-240W-RD design files are currently available for download here: https://www.transphormusa.com/en/reference-design/tdaio-tph-on-240w-rd/.

About Transphorm

Transphorm, Inc., a global leader in the GaN revolution, designs and manufactures high performance and high reliability GaN semiconductors for high voltage power conversion applications. Having one of the largest Power GaN IP portfolios of more than 1,000 owned or licensed patents, Transphorm produces the industry's first JEDEC and AEC-Q101 qualified high voltage GaN semiconductor devices. The Company's vertically integrated device business model allows for innovation at every development stage: design, fabrication, device, and application support. Transphorm's innovations are moving power electronics beyond the limitations of silicon to achieve over 99% efficiency, 40% more power density and 20% lower system cost. Transphorm is headquartered in Goleta, California and has manufacturing operations in Goleta and Aizu, Japan. For more information, please visit www.transphormusa.com. Follow us on Twitter @transphormusa and WeChat @ Transphorm_GaN.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

この記事をシェアする