メインコンテンツに移動

Transphorm's GaN First to Hit Short Circuit Robustness Milestone Key to Motor Drive Applications

Achieved in Collaboration with Yaskawa Electric Corporation, Capability Leverages the Fundamental Advantages of Transphorm's Normally-Off Platform

2023年8月9日

GOLETA, Calif.——Transphorm, Inc. (Nasdaq: TGAN), a global leader in GaN power semiconductors, the future of next generation power systems, today announced it has demonstrated up to 5 microsecond short circuit withstand time (SCWT) on a GaN power transistor with a patented technology. The achievement is the first of its kind on record, marking an important milestone for the industry as a whole. It proves Transphorm GaN's ability to meet the required short circuit capabilities of rugged power inverters such as servo motors, industrial motors, and automotive powertrains served traditionally by silicon IGBTs or silicon carbide (SiC) MOSFETs—an over $3 billion GaN TAM over the next 5 years.

The demonstration was developed with support from Yaskawa Electric Corporation, a long-term strategic partner of Transphorm's and a global leader in low and medium voltage drives, servo systems, machine controllers, and industrial robots. This makes GaN a highly attractive power conversion technology for servo systems, as it allows for higher efficiency and reduced size compared to incumbent solutions. To do that, GaN must pass stringent robustness tests—of which, short-circuit survivability is the most challenging. In case of short-circuit faults, the device must survive extreme conditions with both high current and high voltage. The system can take up to a few microseconds to detect the fault and shut down the operations. During this time, the device must withstand the fault on its own.

"If a power semiconductor device cannot survive short-circuit events, the system itself may fail. There was a strong perception that GaN power transistors could not meet the short circuit requirements needed for heavy-duty power applications such as ours," said Motoshige Maeda, Department Manager of Fundamental R&D Management Department, Corporate Technology Division, Yaskawa. "Having worked with Transphorm for many years, we believed that perception to be unfounded and have been proven right today. We're excited about what their team has accomplished and look forward to demonstrating how this new GaN feature can benefit our designs."

The short-circuit technology has been demonstrated on a newly designed 15 mΩ 650 V GaN device. Notably, that device reaches a peak efficiency of 99.2% and a maximum power of 12 kW in hard-switching conditions at 50 kHz. The device demonstrated not only performance, but also reliability, passing high-temperature high-voltage stress requirements.

"Standard GaN devices can withstand short-circuit for only a few hundredths of nanoseconds, which is too short for fault detection and safe shut-down. However, with our cascode architecture and key patented technology, we were able to demonstrate short-circuit withstand time up to 5 microseconds with no additional external components, thus retaining low cost and high performance," said Umesh Mishra, CTO and Co-Founder, Transphorm. "We understand the demands of high-power, high-performance inverter systems. We have a long history of strong innovation, and we're proud to say that experience helped us bring GaN to the next level. This is yet another validation of Transphorm's global leadership in high voltage GaN robustness and reliability and will be a gamechanger for GaN in motor drives and other high-power systems."

The full description explaining the SCWT achievement, the demonstration analysis, and more is expected to be presented at a major power electronics conference next year.

About Transphorm

Transphorm, Inc., a global leader in the GaN revolution, designs and manufactures high performance and high reliability GaN semiconductors for high voltage power conversion applications. Having one of the largest Power GaN IP portfolios of more than 1,000 owned or licensed patents, Transphorm produces the industry's first JEDEC and AEC-Q101 qualified high voltage GaN semiconductor devices. The Company's vertically integrated device business model allows for innovation at every development stage: design, fabrication, device, and application support. Transphorm's innovations move power electronics beyond the limitations of silicon to achieve over 99% efficiency, 50% more power density and 20% lower system cost. Transphorm is headquartered in Goleta, California and has manufacturing operations in Goleta and Aizu, Japan. For more information, please visit www.transphormusa.com. Follow us on Twitter @transphormusa and WeChat @ Transphorm_GaN.

About Yaskawa Electric Corporation

Yaskawa Electric located in Kitakyushu, Japan, is a world-leading provider of core technologies focused on motion control, robotics, and system engineering. Founded in 1915, Yaskawa Electric has provided exceptional customer experiences for 100 years. Focusing on mechatronic solutions, it has shipped over 20 million AC drives, 15 million servo motors and 300,000 robots worldwide. For more information, visit www.yaskawa.co.jp.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

この記事をシェアする