メインコンテンツに移動

Transphorm's GaN Used in AES' Latest Power Supplies for Large Passenger Airplanes

International Aviation Electronics Supplier Outperforms Competition with GaN-driven Power Density Increases

2024年10月9日

Transphorm Inc.—the leader in the design and manufacturing of the highest reliability and first JEDEC- and AEC-Q101 qualified high voltage gallium nitride (GaN) power semiconductors—today confirmed that customer AES Aircraft Elektro/Elektronik System GmbH has released its first 650 V GaN-based power supplies. Serving the aviation industry, AES supports customers with various products and services ranging from electrical engineering to certification and testing. The company's newest Switch Mode Power Supplies are currently used by large CS-25 airplane manufacturers (e.g., Airbus A318-A321, A330, A340, A380 and Boeing B767, B787 VIP aircraft) and use Transphorm's GaN FETs to increase overall system efficiency by more than 10 percent compared to competitive Silicon-based power supply unites (PSUs).

The two GaN-based Switch Mode Power Supplies are the PS250X 500 W system and the PS6120 1200 W system. Both products support a 96-130 VAC/360 Hz – 800 Hz input voltage with a 28 VDC continuous power output at 15 amps for the 500 W system and 42 amps for the 1200 W system.

Further, AES certified the PS250X and PS6120 as DO-160 compliant—meeting the more than 25-point stringent Standard of the Radio Technical Commission for Aeronautics (RTCA). This Standard assesses system impact and performance under various external and internal conditions on aircraft—ranging from pressure and temperature to voltage spikes and RF emissions.

The flagship 500 W PS250X is the industry's first passively cooled power supply at 420 W and deploys Transphorm's GaN in a single-phase CCM boost power factor correction (PFC) topology. It offers more than 92 percent overall system efficiency at full load, which is more than 10 percent greater than its competition. The system also yields a more than .98 power factor and 200 mVpp nominal at 115 VAC/400 Hz input at full load. All within an end product that is 1.4 kg (~3 lbs).

画像
AES-Transphorm

The 1200 W PS6120 deploys Transphorm's GaN in a fan-cooled, three-phase CCM boost PFC topology. It offers more than 91.5 percent overall system efficiency at full load, which is 11.5 percent greater than its competition. The PS6120 also yields the same power factor and nominal ripple voltage at 115 VAC/400 Hz input at full load as the PS250X 500 W PSU. All within an end product that is 4.0 kg (~8.8 lbs).

"The aviation industry is working toward reducing climate impact through any means possible," said Dr. Andreas Hammer, Head of Competence Center Power, AES. "Considering, we sought out Transphorm's GaN to replace previously used Silicon MOSFETs so that we could provide a more efficient, lighter weight power supply. These supplies have the potential to make a notable impact when considering each aircraft deploys several such PSUs. After only a year of redesign, we were able to offer our customers a better power solution, while also raising the performance bar within our own industry."

The GaN Selection Process

Interested in the technology's inherent higher switching frequency, AES reviewed GaN power switch converters from several GaN device semiconductor manufacturers. The company ultimately selected Transphorm's 650 V GaN technology due primarily to its ease of drivability and designability—specifically because Transphorm's GaN FETs do not require custom drivers. As a result, system design is simplified while engineers can drive the switches using technology they are already familiar with (i.e. drivers and packages). Other factors affecting AES' selection included Transphorm's proven reliability—which is underscored by its GaN platform earning both a JEDEC qualification and AEC-Q101 qualification at 175°C.

"Transphorm designed its GaN devices to enable designers, not challenge them," said Philip Zuk, VP of Worldwide Technical Marketing and NA Sales, Transphorm., "Our two-switch normally-off GaN devices come in standard packages and require minimal supporting circuitry to drive them, which reduces the overall system size, increases reliability, and simplifies design. It's crucial to us that our customers can come to market quickly with a product they have confidence in. We're honored to be AES' GaN supplier of record and are proud that they appreciate the work we've done to bring the benefits of GaN technology to the masses."

AES' PS250X and PS6120 power supplies are currently shipping.

About AES

Headquartered in Germany, AES Aircraft Elektro/Elektronik System GmbH is an international company comprised of over 160 highly skilled employees, serving customers in the aviation, space, and maritime industries. AES' portfolio includes, but is not limited to, aircraft cabins electronics, comprehensive electrical engineering services, electronic design, and certification services.

Welcome to the GaN Revolution!

Transphorm designs and manufactures the highest performance, highest reliability 650 V and 900 V GaN semiconductors for high-voltage power conversion applications. Holding the largest IP portfolio (1000+ issued and pending patents worldwide), Transphorm produces the industry's first JEDEC and AEC-Q101 qualified GaN FETs. This is due to a vertically-integrated business approach, which allows for innovation at every development stage: design, fabrication, device, and application support. Transphorm: moving power electronics beyond Silicon limits. Website: www.transphormusa.com Twitter: @transphormusa


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

この記事をシェアする