メインコンテンツに移動

NLT Technologies Enhances Lineup of Touch Technology Family

19.0-inch High Density and Wide Viewing Angle Model which Is Ideal for Professional Use

2014年5月27日

KAWASAKI, JAPAN, SANTA CLARA, Calif., DUSSELDORF, Germany, May 27, 2014 — NLT Technologies (NLT), together with its sales and marketing channels in the Americas, Tianma NLT America, and in Europe, Renesas Electronics Europe GmbH, has announced the successful development of a new 19.0-inch color LCD module with factory installed projected capacitive (PCAP) touch panel technology.

The newly developed 19.0-inch model is the currently largest size in NLT’s PCAP family, which adapts PCAP touch panel in LCD module, both developed and produced by NLT Technologies. It incorporates NLT’s proprietary Super Fine TFT technology (SFT) that achieves high luminance, wide color gamut and ultra-wide viewing angles and is ideal for use in professional display applications such as medical equipment.

Total touch solution

NLT offers total PCAP solutions, that include the LCD, touch panel and controller board, direct from NLT’s factory. This is important for customers since the PCAP displays are covered by the same factory warranty NLT offers on all of their industrial LCD products. NLT also offers support for drivers and tuning software of touch panel, allowing customers to easily design NLT’s touch panel displays into their end products

Long-term support same as Industrial LCD

NLT’s PCAP products offer the same long-term support program, high quality and Total Cost of Ownership (TCO) benefits as offered for their industrial LCD products.

Various PCAP Options

NLT’s PCAP touch panels offer valuable component and structural options such as bonding, surface treatment, or cover glass. This allows end product designers greater flexibility and more display options depending on the end use of the display.

Recently, the use of touch panel displays with multi-touch functionality is rapidly expanding in consumer applications like smart phones or tablet devices, as well as in industrial and medical applications. The increasing demand for PCAP touch panels continues due to their distinguished image quality, durability, and various construction design possibilities.

NLT Technologies continues to invest and develop new PCAP products. The newly developed 19.0-inch model is the currently largest size in its PCAP family allowing more data to be shown on the display. Furthermore, it incorporates NLT’s proprietary Super Fine TFT technology that achieves high density and ultra-wide viewing angles without compromising brightness or color gamut even in off-angle viewing conditions. Therefore it is expected to be utilized for professional use such as medical equipment.

The prototype of new LCD module will be showcased at Display Week 2014(#1320), June 3-5, at the San Diego Convention Center in San Diego, California in USA.

Main specifications of the new LCD modules can be found in the attachment.

Lineup of PCAP family

About Renesas Electronics Europe’s Display Business

Renesas Electronics Europe is the authorized representative in Europe of NLT Technologies, Ltd. (established July 2011 as a joint venture between NEC Corporation and Shenzen AVIC Optoelectronics, Ltd.), a leading supplier of innovative LCD products for industrial applications. With an extensive lineup of 3.5- to 22.5-inch active-matrix LCD modules and a network of distributors, Renesas Electronics Europe provides complete display module solutions from NLT Technologies to the industrial, medical and high-end monitor market. In addition to modules based on NLT Technologies' SFT for ultra-wide viewing, Renesas Electronics Europe also offers LCD modules that include ultra-high resolutions, wide temperature ranges, high contrast ratios, rich color gamuts, backward compatibility, LED backlights, and transflective viewing for use in diverse lighting environments.

Renesas Electronics Europe and NLT Technologies are committed to delivering innovative, high-performance, eco-conscious LCD solutions that address the diverse size, power and high image-quality needs of their industrial, medical and high-end monitor customers. Based on technologies developed by NLT Technologies, the LCD modules are optimized and designed for a range of applications, including portable and fixed medical equipment, test and measurement devices, instrumentation equipment, point-of-sale systems, gaming systems, global positioning systems, factory automation and barcode scanners.

Additional information about these LCD display products, manufactured by NLT Technologies and represented by Renesas Electronics can be found at www.renesas.eu/display


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

この記事をシェアする