NOTE:
1. The logging process is on hold while the label is connected
2. Erase the logged data before disconnecting for correct timestamping and logging
3. Set and verify the system time
4. Do not trigger a new command while a previous one is active
Simple steps to follow:
- Press the push-button on the label for >3s and release.
画像

- To turn the label off, please connect the label to a device running the web-app by scanning for and connecting to the label first and pressing the off-button.
- Scan for labels and pair to read the logged data.
Bluetooth LE SmartLabel Logger SUOTA - US207
Configuration | ||||
Device Name: | ||||
Transmit Power (dBm): | ||||
Measurement Period (ms): | (minimum = 5000ms) |
|||
Time: | ||||
Live Measurements | ||||
Battery Level (V): | Capacity (%): | |||
Accelerometer (G): | ||||
Temperature (℃): | Humidity (%RH): | |||
Sensor Log | ||||
Log Size (bytes): | ||||
Log Used (bytes): | ||||
Firmware | ||||
Firmware Version: | ||||
Firmware Image: | ||||