メインコンテンツに移動

GUIX Hello World for the SK S7G2 Starter Kit

2018年6月22日

The purpose of this training is to guide you through the setup of a GUIX touch screen interface “Hello World” application in e2 studio. The supporting documentation covers all configuration steps including setting up the hardware function, threads, interrupts, LCD driver and touchscreen on a SK-S7G2 Starter Kit.

Transcript

Optional Transcript goes here if available. Read through the transcript text and link any appropriate keywords and products that have pages.

Example:

There are many 12V rails in industrial applications today that need a buck converter to step the voltage down to a lower voltage and deliver up to 14 amps. The ISL85009, ISL85012 and ISL85014 are pin compatible, very efficient and are able to deliver up to 14 amps.