メインコンテンツに移動

TARA Embedded Wizard Graphical User Interface on RZ/A Stream it! - RZ - V2.0!

2018-10-25

Welcome to this demonstration of TARA Embedded Wizard on Renesas' new solution kit Stream it! - RZ-V2.0. The Stream it! - RZ-V2.0 is based on RZ/A1-LU MPU, which runs at 400MHZ, provides 3MB of embedded SRAM and is optimized for HMIs from the ground up. Embedded Wizard is TARA Systems' embedded GUI technology that enables you to create platform-independent and high-performance graphical user interfaces, even on resource constrained microcontrollers.